Technical FAQs

Ask a Question

Filter results

    How can I mass configure an Network Management Card (NMC) or NMC embedded product?
    Method 2 - InfrastruXture Central/StruxtureWare Central/StruxureWare Data Center Expert
    Video: Data Center Expert | How do I configure the network settings?
    1) and log into the DCE Client software. 2) Navigate to the System Menu > Server Administration Settings > Network Settings .
    How do I mass configure APC user settings using Data Center Expert?
    StruxureWare Data Center Expert (DCE) APC Network Management Cards (NMC)
    Video: Data Center Expert | How do I mass configure APC devices?
    - Virtual Appliance (AP94VMACT) APC Network Management Cards (NMC)
    Video: Data Center Expert | How do I configure auto-login when launching to APC devices?
    - ISXC, SWC, & DCE (all versions) - APC Network Management Cards (NMC)
    Video: Data Center Expert | Backing up to a Windows Share
    (Hostname can be used if DNS is configured in System > Server Administration Settings > Network Settings )
    Data Center Expert | How do I restore to defaults and restore a backup?
    NOTE: Keep in mind any IP Address restrictions within the network management cards SNMP settings or network firewalls that may prevent communication from working properly.
    DNS may not work properly after firmware upgrade on Network Management Card 1 (NMC1) when using DHCP boot mode
    ... .) StruxureWare Data Center Expert users can push out a configuration template with the DNS server information from DCE's APC SNMP Device Configuration feature.
    Video: Data Center Expert | Managing Users
    - The client computer must have access on the network to the Authentication server as it is performing the connection during the configuration .
    Results 1 - 10 of 50