Technical FAQs

Ask a Question

Filter results

    Video: How do I configure StruxureWare Data Center Expert to send e-mail notifications?
    Click on Alarm Configuration drop down menu Select Manager Alarm Action
    Video: How do I customize short message e-mail alarm actions in Data Center Expert?
    Resolution: 1) Open the DCE Client and go to: Alarm Configuration menu > Manage Alarm Actions .
    What type of information can I see in a NetBotz SNMP trap?
    This is the same when configuring traps for StruxureWare Data Center Expert (DCE) using the alarm action configuration for a trap.
    Can a NetBotz configuration backup be used on another NetBotz appliance?
    ... appliance, some settings such as alert actions or user login information will get transferred to the new appliance but any configuration for thresholds or ...
    Alert Actions for NetBotz Version 2 Appliances
    ... 1 Trap Sends an SNMP version 1 trap to configured targets none Send HTTP POST Sends standard (all) alert information formatted
    NetBotz v3 | How do I configure a PCNS Shutdown alert action?
    For more information , see the documentation for PowerChute Network Shutdown v4.2.
    Data Center Expert | How do I disable/suppress alarms?
    ... Process for disabling alarms in StruxureWare Data Center Expert StruxureWare Data Center Expert (DCE) StruxureWare Data Center Expert (all versions ... ... disabling and suppressing alarms in DCE: ... Mode, no alerts , for that ... out for the alarm actions defined in the ... ... still see the alarms , and record them within Alarm History, but no actions will take place ... ... that will generate alarms . ... , the device information will appear faded ... ... notifications sent from Data Center Expert . Alarm Suppression: When an alarm is present in Data Center Expert , future notifications ...
    What type of information is provided in an SNMP trap from StruxureWare Data Center Expert?
    ... What type of information is provided in ... trap from StruxureWare Data Center Expert ? ... StruxureWare Central / Data Center Expert StruxureWare Data Center Expert any version ... using the " Alarm Action " functionality as ... ... upon both manually configured thresholds under the "Threshold Alarm Configurations " tab as ... pre-created alerts (Essential alerts ) that are ... the "Device Alarm Configurations tab. ... are using an alarm action , the traps ... ... be version related info as well so ... ... also provide additional information / arguments as ... ... : An ISXC Alarm exists. ... the unique ISXC alarm ID.
    Voicemail Alert Action using IPing
    Voicemail Alert Action using IPing The Iping information can be found ... ... -Mail" Alert Action and customizing it ... ... that the same alert action can be used ... Message pane when configuring this Alert Action ). Test the alert action until the message ... ... pane of the Alert Action : ... individual sensor's threshold setting (Advanced tab ... ... to make the alert more natural sounding ... The e-mail address in the alert action should be specified as "ping.xxx-xxx-xxxx@iping.com" where xxx-xxx-xxxx is the phone number (with area code) of the alert recipient.
    How do I Configure NetBotz appliances to send e-mails on an alert?
    ... threshold is in alarm . ... threshold is in alarm the follow option must be configured . ... associated to a Alert Profile The Alert Profile must have an Alert Action The Alert Action must have the correct email address configured ... to test and configure email notification within ... ... be able to configure and test email actions . ... and Testing Email Settings ... Click on the Configuration icon located at ... ... Under the Appliance Settings click on E ... ... -mail server information is correct ... and test email alert actions ... Click on the Configuration icon located at ... Select Alert Actions ... and click Test alert .
    Results 1 - 10 of 50