Technical FAQs

Ask a Question

Filter results

    INFORMATION BULLETIN: Network Management Card 2 upgrade from v5.1.X to v6.0.6 incorrectly maps SMTP server information
    Devices with an embedded Network Management Card 2 include (but are not limited to): 2G Metered/ Switched Rack PDUs (AP86XX, AP88XX, AP89XX), Certain Audio/Video Network Management Enabled products. ... Users using "Local SMTP server" setting for email notifications ... Change the "Server" setting to Custom, or Copy the mail server information from "Custom SMTP server" to "Local SMTP Server" ... Also, please review for a related issue regarding email notification settings and the config .ini
    How To: Configuring an APC Network Management Card with popular email services such as Gmail, Yahoo!, Office 365, and Hotmail/Outlook.com
    ... time; local mail server is not available to relay mail to an external ... ... : Metered/ Switched Rack PDUs ( ... Rack Automatic Transfer Switches (AP77XX, ... ... G Metered/ Switched Rack PDUs ( ... ... sent using external mail services. ... test using the configured DNS servers to ... Configure the "From ... ... is recommended you change the from address ... ... required for other mail services as well ... Configure the other email ... ... using the local mail server, changing your "From ... cause your local mail server to reject ...
    Unlicensing a Camera from NetBotz Central Results in Deletion of Associated Surveillance Pictures
    StruxureWare Data Center Expert ... When a camera is unlicensed from NetBotz Central/ StruxureWare Data Center Expert Surveillance, any existing Surveillance pictures associated with this camera is purged from the server's database. To retain the historical Surveillance pictures for a camera without having it posted future Surveillance pictures to the server, set " Post Mode" to 'Disabled' in Modify Camera Surveillance Settings . This way, no more new Surveillance pictures are generated from the camera, and users can still review past Surveillance pictures associated with this camera.
    Issues with NetBotz Appliances in Post-Only Mode and Some Firewalls
    The solution is to change the configuration on the firewall to not remove unknown / proprietary headers or not drop packets with this information .
    Issues with NetBotz Appliances in Post-Only Mode and Some Firewalls
    Resolution: The solution is to change the configuration on the firewall to not remove unknown / proprietary headers or not drop packets with this information .
    How do I troubleshoot email failures on a Network Management Card?
    ... : Metered/ Switched Rack PDUs ( ... Rack Automatic Transfer Switches (AP77XX, ... ... G Metered/ Switched Rack PDUs ( ... ... including the NMC's mail server setting , DNS configuration , or network ... Review the sections below ... ... .txt, data .txt and config .ini ... NMC device and mail server that you ... ... Local Email Server setting In configuring the email for ... the basic networking information if it is ... the DNS server information needs to be ... on the DNS configuration page. ... the DNS server information has not been ... ... the DNS server information and ensure he ...
    APC Security Advisory - InfraStruxure Central 5.0 Java Runtime Environment
    ... processing of XML Data . Problem Summary ... processing of XML data may allow unauthorized ... ... with processing XML data may allow an ... ... of malicious XML data ... system administrator manually configures the system to ... ... uploading of XML data , the data must adhere to ... Problem Summary ... system administrator manually configures the system to ... Problem Summary ... applet to access information from another applet ... ... system administrator manually configures the system to ... Problem Summary Problem Summary Problem Summary Problem Summary ... system administrator manually configures the system to ... Problem Summary ... system administrator manually configures the system to ... ... IS SOME MATERIAL CHANGE IN THE FACTS ...
    Network Management Card 2 (NMC2) v6.X.X potential reboot loop or TCP/IP stack failure experienced when SMTP server MX record is not cached on user's DNS server
    ... of connectivity after configuring SMTP settings or where an ... the user's notification settings . ... G Metered/ Switched Rack PDUs ( ... ... Users attempting to configure SMTP/email ... NMC2 querying a mail exchange server that is ... a user has configured (meaning the ... Once the mail exchange server is cached ... Review your event. ... ... txt should be reviewed to see if ... ... of connectivity after configuring SMTP settings or where an ... the user's notification settings . ... txt should be reviewed and analyzed to ... ... v5.1.X firmware for your application while reviewing the information and support for downgrading ...
    Post-Only Mode Overview with StruxureWare Data Center Expert
    Post -Only Mode Overview with StruxureWare Data Center Expert StruxureWare Data Center Expert StruxureWare Data Center Expert Posting configuration options Post -only mode ... ... with the newer Data Center Expert systems Post -only mode ... Central or StruxureWare Data Center Expert. When in Post -only mode ... ... server, all data collected by the ... jobs such as changes or updates. Note: When viewing current sensor readings and pictures for Post -only appliances, the data can be up to 30 minutes old by default as it is pulled from the database and is not live/real-time.
    Configuring Post-only Mode for Netbotz Version 2 and 3 Appliances
    Configuring Post -only Mode ... StruxureWare Data Center Expert. NetBotz posting configuration . ... NetBotz appliance can post . ... be placed in Post -only mode ... ... an appliance in Post -only Mode ... ... ” then “ Post Only Mode” ... ... will be " posting " to as ... the appropriate authentication data . ... Central or StruxureWare Data Center Expert server. ... ... all of the information is correctly entered ... ... appear with status information . ... on the " Post to INfraStruxure Central ... and ensure the information is correctly entered ... ... If the initial post is successful then the stats will change to "Registered ...
    Results 1 - 10 of 50