Rack PDU 2G (AP8XXX) Network Port Sharing Information
... ability to share one IP address via one network connection) ... PDUs using only one ... functionality of v 6 .X. ... ... a number, 1 to 4, ... ... are connected to one another in a ... ... 0w05545a which includes qty 2 terminators and ... ... total length of cabling connecting Rack PDUs ... ... " port of one of the grouped ... ... desired order, 1 to 4. ... ... have Display ID 1 . ... access to outlets 1 , 2, ... 3 on unit 1 , ... 2, outlets 1 through 6 ... , and outlets 1 ,2,4 through 6 , 7 through ...