Technical FAQs

Ask a Question

Filter results

    SurgeArrest - minimum install distance of 10 meters (30ft).
    ... between the electrical outlet and the electrical ... APC Surge Arrest products ... Type 1- 5 . ... downstream of the main overcurrent protective device ... ... utilization equipment being protected . ... or more Type 5 components together with ... ... external short circuit protection . Type 5 ... to the voltage protection rating ... UL96A "Lightning Protection Systems" specifications ... ... ) from the main electrical service panel ... ... for direct lightning protection , therefore it ... It is important to note that ... downstream from the main service panel. Ideally for residential use, Type 2 which is often referred to as "TVSS" protection should always be installed at the main electrical service entrance.
    Why is the Protection Working LED of an APC SurgeArrest, or SurgeProtector off?
    illuminate: 1. The unit is powered off (for 7 outlet SurgeArrest strips only).
    Video: What does the Site Wiring Fault Indicator LED on my APC UPS or Surge Arrestor represent?
    All 120v APC Back-UPS and SurgeArrest products ... -UPS and SurgeArrest products equipped with ... On APC UPS products this ... APC recommends that you ... ... wire (> 5 Volts AC measured ... If the outlet that the APC UPS unit is ... Therefore, in order to maintain your warranty and protection under APC's Equipment Protection Policy, be sure that the APC unit is only plugged into a properly grounded outlet where the Site Wiring Fault Indicator (SWF) light is not illuminated.
    Cable Picture Degradation When Using an APC Coaxial Surge Protector
    After connecting an APC device with Coax Protection , customer observes picture degradation or loss of digital channels. ... SurgeArrest , Protectnet, Back-UPS, Back-UPS Pro, APC AV line of products ... Inserting a cable protector like an APC ... APC Coax protection has been tested from 30 MHz to 1 GHz. It's insertion loss is at 1 GHz were attenuation is 5 dB. ... terminated cables from an electronics store ; such as Radio Shack. ... (available at many electronics stores ).
    Proper installation of a telephone line into an APC product with telephone line protection.
    ... side of a telephone patch cable to the telephone jack in the ... jack on the APC product (" ... ""Wall outlet "" or ...
    APC Switched Rack PDUs - any pending outlet commands are lost when PDU Network Management Interface is rebooted
    ... powered by an outlet ... Users turning the outlet off for more ... ... Rack PDU with outlet commands pending Pending outlet commands are stored by the Rack ... ... in , pending outlet commands may be lost and outlets will not perform ... ... watchdog mechanisms to protect itself from becoming ... ... take 3- 5 seconds each depending ... or how many outlets you are applying ... ... same Rack PDU's outlets (and turn ... ... unaffected when controlling outlets on a particular ... ... Interface while any outlet commands are pending ... - Any pending outlet command will be ... next to the outlet in the web ...
    Where can I get support for APC and MGE Products?
    For support on APC and MGE products please visit: http://www. apc .com/support/ ... APC CS APC Enterprise Manager APC ES APC RS ... Biometric Security ... Metered-by- Outlet Rack PDU ... Notebook Security ... Security Cameras ... SurgeArrest Essential SurgeArrest Home/Office SurgeArrest Notebook SurgeArrest Performance
    Recommendations for protecting a laser printer
    What are APC's recommendations for protecting Laser Printers? SurgeArrest , Back- ... ... these devices, APC does not recommend protecting laser printers with ... ... a UPS's Battery Outlets OR in to its Surge Only Outlets . These low voltage situations may cause an APC Back-UPS to transfer to battery operation repeatedly, eventually exhausting the unit's internal battery unnecessarily. ... If you must use a UPS with a Laser Printer it is important to size your UPS appropriately. APC recommends a Smart-UPS series product that is sized for the maximum power draw of the laser printer as defined by the manufacturer.
    Did APC purchase the AirFlow Company?
    Did APC purchase the AirFlow ... APC purchased Airflow in ... Air Division under APC . American Power Conversion Expands Availability Solutions with Acquisition of Airflow Company ... will operate within APC’s Availability Enhancements Group, further strengthens APC’s stature as a ... one-stop shop of availability solutions ... ... Jr., APC’s president and CEO ... ... The marriage of APC and Airflow is ... win, providing APC with entry into ... business while leveraging APC’s global scale, ... ... to industry and APC estimates, Airflow ... ... enhance availability of critical IT and telecommunications ... equipment it is protecting . ... Since 1997, APC has made a ... ... to standardize on APC for virtually all ...
    Video: Why might my APC Back-UPS Product be beeping?
    APC's UPS Selector ... removing non- essential equipment. ... you want to protect , visit 5 .) Disabling ... ... 1 beep every 5 seconds ... unit shipped with APC management software it ... ... section of the APC management software for ... ... + or - 5 % this will ... ... is 3 to 5 times the size ... ... +/- 5 % deviation. ... automatically if the APC management software is ... ... from the wall outlet contact APC Support APC's UPS Selector. ... ; Repeated Every 5 Hours (Replace ... ... of the battery outlets ).
    Results 1 - 10 of 50