Technical FAQs

Ask a Question

Filter results

    ACSC1XX Spare Parts List
    CABLE ASSY TEMPERATURE SENSORS (Rack Inlet) 0J-0w2818a { 13FT .EN_US}
    Video: How do I configure APC Network Management Card network settings?
    ... a DB- 9 serial port 940 ... (DB- 9 to DB- 9 ) Rack PDU ... ... to DB- 9 ) 1st Generation ... (DB- 9 to DB- 9 ) 2nd Generation ... to DB- 9 ) 4th Generation ... ... to DB- 9 ) Netbotz 200 ... (DB- 9 to DB- 9 ) Rack Air ... (DB- 9 to DB- 9 ) ... <Enter> 3 -5 times ... ... 2.5mm jack labeled "console ... Press enter 3 -5 times ... ... boot mode to m
    Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
    Symmetra 3 phase (Symmetra ... ... Management Card v 3 .X. ... /8/ 9 ... AP9619 use firmware 3 .X and ... 3 . From the ... ... files for the three firmware modules follow ... ... the RJ- 45 Ethernet jack , will begin ... ... firmware version for three seconds and then ... ... -enter Parameters 3 ) Quit. 3 . Open a ... ... . Select option 3 - System. 9 . Select option ... 3 . Run a ... ... the DB- 9 serial port at ... ... the DB- 9 serial port of ... 3 . Open an ...
    What are the requirements for the acsc100 condenser unit
    The SC condenser section normally moves up to 1440 m 3 /hr (850 CFM), ... With a 9 C delta I would estimate that the condenser exhaust temperatures would be approximately 37 C and 41 C respectively. ... 0. 45 ... Condenser Air Flow Rate SCFM ( m 3 /hr)
    Why does my local mouse (the mouse on the server I am connecting from) not synchronize with my remote mouse (the mouse on the server I'm connecting to) when connected through the APC IP KVM product?
    Solaris 9 ... From the Workspace Menu, select Desktop Manager and go to step 3 - or - ... : xset m 1 ... : xset m 0 or xset m 1 (if one doesn't help, try the other.) ... : xset m 1 ... Server module part number (Server modules are the components that connect the from the RJ- 45 port on the KVM to your remote server).
    Where can I get support for APC and MGE Products?
    ... 25 0033- 3 0033-50 ... 100 0034- 3 0035-100 0035-2 M -E 0035- 3 0035- 3 M -E 0035nd-2 M -1E 0035nd- 3 M -1E ...
    NetBotz 455 | Physical Description
    NetBotz version 3 3 Power LED Indicates ... 1 Microphone jack Supports audio sensing, audio recording, and two-way audio. Maximum length of microphone cable: 3 m (9.8 ft). 2 Speaker jack Supports two-way audio. ... Maximum length of speaker cable: 3 m (9.8 ft). 3 A-Link port Used for cascading NetBotz sensor pods and temperature and humidity sensors with digital displays.
    How do I reset the communication card of a SmartCell XR?
    ... from the OUTPUT jack on the rear ... 3 . Use a pointed object (i. e. paper clip, fine ball-point pen) to press and hold the reset button located between the communication jacks on the rear of the battery pack. 4. While pressing the reset button, reconnect the battery communications cable to the OUTPUT jack . ... 8. Reconnect (do not press the reset button this time) the battery communications cable to the OUTPUT jack . ... 9 . The Replace Battery indicator should be out.
    Video: Network Management Card (NMC) Password Reset Procedure
    3 .) ... a DB- 9 style serial port ... For three phase UPSs, it will be necessary to remove the communication cable from the port labeled "Display" that connects to the PowerView display prior to completing this reset procedure. ... The terminal settings are correct as specified in step 3 . ... 9 .) ... You'll also need to press the pinhole reset button - access is located on the front of the Network Management Card to the right of the Ethernet jack . ... 3 .) ... The terminal settings are correct as specified in step 3 .
    Serial Communication Cable used for SURTD model UPS models
    The SURTD online UPS models use an RJ- 45 to DB- 9 Serial Cable.
    Results 1 - 10 of 50