Why choose glycol over water?
Why choose glycol over water ? ... All cooling units that require heat exchangers ... Why choose glycol over water ? ... There is a one-time initial cost to fill the system with 30 -40% glycol. ... - Glycol is 5-10% less efficient than water in transferring heat. ... Note! of an based water solution is less ... than the specific heat of clean water . ... Distilled or deionized water should be used for ethylene glycol solutions. City water is often treated with chlorine, which is corrosive, and should be avoided.