Technical FAQs

Ask a Question

Filter results

    How do software support contracts work for StruxureWare Data Center Expert.
    How do software support contracts work for StruxureWare Data Center Expert . StruxueWare Data Center Expert . Struxureware software support contracts for version 7 ... ... server is under software support can be confusing ... ... server has enough software support . StruxureWare servers do not have any software support "out of ... ... must be under support in order for ... upgrades for their StruxureWare server or even ... Software support contracts are required for ... ... not currently require support contracts . ... that the server support contracts such as WMS1YRBASIC ... ... have an AP9465 StruxureWare Data Central Basic with an additional ... to be under support for a year ...
    Why does StruxureWare Data Center Expert not accept my One Time passcode?
    StruxureWare Data Center Expert is not accepting ... StruxureWare Data Center Expert StruxureWare Central / Data Center Expert all versions. SturuxureWare Data Center Expert requires a 64 ... passcode and the Data Center Expert's MAC address. 1 . In a ... AP9465 = StruxureWare Data Center Expert Basic ap9470 = StruxureWare Data Center Expert Standard AP9475 = StruxureWare Data Center Expert Enterprise AP94VMACT = StruxureWare Data Center Expert Virtual Machine SFDCOBASE = StruxureWare Data Center Operation ... a VM or Data Center Operation. ... all the relevant information . ... a word processing application such as notepad ... ... . Launch your Expert client.
    StruxureWare Data Center Expert v7.4.2 is no longer available
    Resolution You must have a valid support contract to receive the software update.
    How can I resolve “Failed to create java virtual machine.” error when launching StruxureWare Data Center Expert client?
    1 ) Navigate to ... Installation directory for StruxureWare Data Center Expert . (default ... C:\ Program Files (x86)\ StruxureWare Data Center Expert X.X ...
    Video: Where can I download the StruxureWare Data Center Expert client software?
    Resolution: 1 ) Open the DCE Appliance web interface by entering the IP address or hostname in a web browser.
    Data Center Operation | Video: Copying files from the StruxureWare Data Center Operation
    1 . Open the application 2. Enter IP address or hostname within the "Host Name" field
    Restoring StruxureWare Data Center Expert backup to a new Virtual Machine causes system to not fully boot up.
    Restoring StruxureWare Data Center Expert backup to a ... StruxureWare Data Center Expert StruxureWare Data Center Expert Virtual Machine ( ... Migrating a StruxureWare Data Center Expert hardware server to ... ... equivalents for the StruxureWare Data Center Expert Basic , Standard, ... ... , and the StruxureWare Data Center Expert virtual appliance will ... 1 . Gracefully shut down the virtual appliance. ... See StruxureWare Data Center Expert virtual server equivalent configurations. ... Changes in the disk space will take effect once the StruxureWare Data Center Expert virtual appliance has restarted. ... To store large amounts of surveillance data , using a remote repository is recommended.
    How do I obtain an SNMP or Modbus DDF for StruxureWare Data Center Expert to monitor 3rd party devices?
    ... a DDF for StruxureWare Data Center Expert to monitor 3rd ... StruxureWare Data Center Expert (DCE) StruxureWare Data Center Expert (DCE) ... to your DCIM Support account at ... computer the client application is installed on ... 1 ) Within the ... and select DCIM Support Community. 2) Select Yes to associate your DCE appliance to your DCIM Support account. ... If you do not have an account, register for one before continuing. ... 4) Select Device Support on the Navigation bar. ... You can then select "I Want it too" within the Data Center Expert entry. ... 7) Fill in the required information .
    Why isn't my DNS change saving in StruxureWare Data Center Expert?
    Changing DNS entries in StruxureWare Data Center Expert UI for VM does not save changes. ... StruxureWare Data Center Expert ... StruxureWare Data Center Expert VM with single NIC configured ... It has been seen where changing a DNS entry in StruxureWare Data Center Expert (DCE) when using the console application does not cause the system to reboot and save the DNS changes. This only happens on a system with a single NIC so it is not seen on the DCE hardware servers, only on a DCE VM server.
    Can StruxureWare Data Center Expert output a 32 bit register with its Modbus output?
    A single register in StruxureWare Data Center Expert's modbus output is ... StruxureWare Central / StruxureWare Data center Expert StruxureWare Central any version StruxureWare Data center Expert any version ... output of a single register for StruxureWare is a 16 ... ... handled by a single register. ... bit register in StruxureWare . ... this limitation, StruxureWare Data Center Expert can be configured ... StruxureWare does not know ... ... value of either 1 or 2. ... ... , the polling software must be reconfigured ... 31000 returns 0000000000000001 If this were a single register, = 1 ... This math must all done on the side of the querying application .
    Results 1 - 10 of 50