StruxureWare Central (SWC)
InfraStruXure Central (ISXC)
NetBotz 700 Series
- NetBotz Rack Monitor 750 (NBRK0750)
Environment:
NetBotz 750 / 755 version 5.2 firmware with a camera pod 165 in Surveillance View of DCE 7.7
Cause:
Cameras are added to DCE in a different manner on a NetBotz NBRK0750 or NBWL0755
Resolution:
When you remove a version 2 or 3 NetBotz appliance with a camera pod 120 or 160 from a DCE server, the camera thumbnail will automatically be removed with the device. This is not the case with the NetBotz camera pod 165. Even after you remove the appliance from the monitoring perspective of DCE, the camera thumbnail will remain. To remove this thumbnail, you must right click the image and choose the "Delete" option.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.