Browse FAQs

Local NetBotz Camera Pod 165 Does not Appear in the Appliance Web UI

Published date: 16 July 2020

Issue:
If you move the camera pod from your company network (a remote connection) to the appliance’s private network (a local connection), the camera pod does not appear in the Web UI of the appliance.
 
Product Line:
NetBotz 5.x
NBPD0165
 
Cause:
The camera pod retains the IP address lease from your company’s network for a period of time (which varies by company) before it acquires a new DHCP lease from the appliance. Until the Camera Pod acquires a new lease from the appliance, it does not appear in the Web UI
 
Resolution:
Reset the Camera Pod 165 to force it to acquire a new lease immediately. Press the reset button for at least 30 seconds (until the top Network LED on the camera pod turns off). Then wait about 5 minutes for the appliance to reconnect to the camera. Do not disconnect the camera pod from power during this time.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.