Samsung Lithium Ion Battery; alarm status-LED indication
Published date:
01 August 2018
Issue: Samsung Lithium Ion Battery; alarm status-LED indication
Product line: Samsung Lithium Ion Battery
Environment: All models, all serial numbers
Cause: When the operating limits of the LIB system are exceeded, the system will protect itself from failure. System has been programmed with conditions and setpoints (e.g., over voltage, over temp) that create an Alarm or Fault state. System provides indications and information about its health and operational status via LEDs on the BMS.
Resolution: See chart below of alarm LEDs:
Resetting the System: Reset system after release conditions are met by pressing and holding RESET button for 3-to-5 seconds on the SMPS assigned as System BMS.
If you cannot reset the alarm condition or require further support please call Schneider Electric Technical Support 877-537-0607
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.