Browse FAQs

Video: How to change the Display password Timeout settings on a Network Air FM unit

Published date: 20 July 2020

Issue:
This dcoument contains a video that will describe how to change the Display password, Timeout settings on a Network Air FM unit.
 
Product line:
FM 35-50, IR40, ACFM400, ACFM200.
 
Environment:
All Serial Numbers.
 
Cause:
Install, Configuration.
 
Resolution:

  1. Press the ESC Key until you get to the main menu.
  2. Press ENTER on Setup.
  3. Press ENTER on System 1.
  4. Press ENTER on Display.
  5. Press ENTER on Password & Timeout.
  6. Using the UP or DOWN arrows you can select the Timeout (This will allow the amount of time on the display before you will have to enter a password again).
  7. Press ENTER and now you will need to enter a password.
  8. The default password is 7852 Select each number and then press ENTER to move to the next one.
  9. Press ENTER again and you can change the time from 1 min to 4 hours.
  10. Press ENTER and the ESC back to the status menu.
  11. Finish by pressing the ENTER key and then press ESC until you get to the status menu.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.