What are the BTU/hr rating for NetBotz appliances?
Published date:
25 January 2017
Issue:
What are the BTU/hr rating for NetBotz appliances?
Product Line:
Netbotz Appliance
Environment:
Netbotz Appliance Version
Cause:
When building a data center, cooling is a key factor to maintain proper operational temperatures. This article contains the BTU/hr rating for NetBotz appliances.
Resolution:
The information below contains calculations for a fully populated NetBotz Appliance
NetBotz Rackmonitor 450/550
Part Number NBRK0450, NBRK0550
Max Power Draw = 240W
BTU/hr = 800
NetBotz Rackmonitor 570
Part Number NBRK0570
Max Power Draw = 480W
BTU/hr = 1600
NetBotz Wallmonitor 355/455
Part Number NBWL0355, NBWL0455
Max Power Draw = 12.0W
BTU/hr = 40.94
The following formula was used to calculate BTU/hr
P(BTU/hr) = 3.412141633 × P(W)
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.