Can the NetShelter cabinet lay flat during shipment?
Published date:
11 March 2019
Issue:
Customer is asking if the NetShelter cabinet may be tilted or lay flat on it's side.
Product Line:
NetShelter SX, NetShelter SV, NetShelter VX, NetShelter AV
Environment:
All versions and serial ranges.
Cause:
In order to save space, or fit into an oddly shaped freight container (like an air freight container), someone may wish to lay the NetShelter cabinet flat.
Resolution:
Absolutely not. A NetShelter cabinet is never to be tilted or laid flat during transit.
The only exception is the AR2400FP1 which ships unassembled, and can lie flat during transport.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.