Using Symmetra RM outside of a Rack (Symmetra RM Floor Mounting Kit)
Published date:
17 December 2014
Issue:
I do not want to mount Symmetra RM in a rack; I want to put it on the floor. What are my options?
Product Line:
Symmetra RM
Environment:
All serial ranges
Cause / Overview:
Some applications require that a Symmetra RM UPS not be mounted in a rack. This article details the options that are currently available to the customer.
Resolution:
There is an optional floor mount kit available for the Symmetra RM UPS, SYOPT1. This can be used to install the UPS chassis in a tower configuration and is the only approved method to do so. More information can be found at the following links:
Please Note: The SYOPT2, SYOPT10, and SYOPT11 that are mentioned in the guide have been DISCONTINUED and are no longer available. The SYOPT1 is the only piece of the floor mount kit currently available.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.