Browse FAQs

How to Display firmware identification number on an EcoBreeze Expansion Module.

Published date: 05 June 2020

                                                                                                                                                           

Issue:   
This article explains how to Display firmware identification number on an EcoBreeze Expansion Module.

Product line:
ACEC200, ACEC201. 

Environment:  
All serial numbers. 

Cause:  
Install. 

Resolution:    

On switch-on, during the start-up test phase, holding the DOWN button, the project identification is displayed for about 2 seconds. The information regarding the

versions/revisions of the project is displayed in sequence. The procedure is exited automatically at the end of the start-up.

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.