Technical FAQs

Ask a Question

PowerChute Business Edition loses communications with HP ProLiant server

Issue:
PowerChute Business Edition loses serial communications with HP ProLiant server

Product:
PowerChute Business Edition (PCBE)

Environment:
HP ProLiant server with Integrated Lights-Out (iLO) enabled

Cause:
Integrated Lights-Out (iLO)

Solution:

HP did provide knowledge base document http://h20564.www2.hpe.com/hpsc/doc/public/display?docId=emr_na-c00843255&sp4ts.oid=398220

Or for continuous data transfer through the Serial COM port, use the procedures provided below to reset iLO:

1. Power on the server.
2. Browse to the Integrated Lights-Out (iLO) Web-based interface IP address using a Web browser.
3. Login to Integrated Lights-Out (iLO).
4. Click on the Administration tab.
5. Click on the Network Settings link in the left side frame.
6. Click on the Apply button at the bottom of the Network Settings web page.
7. iLO will reset and the COM port will release.


For Gen10 UEFI BIOS.
1. System Configuration  >  BIOS/Platform Configuration (RBSU)  >  System Options  >  Serial Port Options  >  Virtual Serial Port >> set it to disable.
2. System Configuration  >  BIOS/Platform Configuration (RBSU)  >  System Options  >  Serial Port Options  >  Embedded Serial Port >> set it to disable.
If point # 2 disables serial port from OS it is recommended to set it to COM1. Leaving VSP port in disabled state.

Please review the HP support document for assistance.

https://support.hpe.com/hpsc/doc/public/display?docId=emr_na-c01139344

 

Was this helpful?
What can we do to improve the information ?