Browse FAQs
Whether to install a suction line drier or liquid line drier
Published date:
14 August 2013
Browse FAQs
Issue:
Whether to install a suction line drier or liquid line drier
Product line:
All Air Cooled Units
Environment:
All Product models, all serial numbers
Cause:
Remove contaminants from system
Resolution:
It is imperative for the technician to allow a minimum of 48 hours of unit operation before the liquid line filter-drier or the suction line filter-drier. After the cleaning procedure is completed, recheck in approximately one to two weeks to ensure that the system condition and operation is completely satisfactory.