Using PowerChute Network Shutdown in a redundant UPS Scenario
Published date:
02 June 2020
Issue:
The purpose of using Power Chute Network Shutdown with a redundant UPS configuration is to confirm that an event is occurring on all UPS before sending a shutdown signal to the connected servers.
Product Line:
Power Chute Network Shutdown
Environment:
All support OS
Cause:
Informational
Solution:
Information concerning configuring PCNS with redundant UPS can be found at this link Application Note #98
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.