Telephone/DSL Splitter of the S15 & S15BLK, AV Power Conditioner w/ Battery Backup.
Published date:
23 January 2018
Issue:
The S15, Power Conditioner with Battery Backup has a Telephone/DSL line splitter, along with COAX and Ethernet surge protection
Product Line:
S-Type Power Conditioner w/ Battery Back-up.
Environment:
S15, S15BLK
Cause / Resolution:
The Telephone/DSL splitter will accept a 2-line 4-wire telephone connection and splits it off into two separate telephone lines. When a telephone connection comprised of two separate telephone lines, is connected to the Telephone/DSL splitter, line ONE will be split to ""Out A""(pins 2&3) and line TWO will be split to ""Out B""(pins 2&3).
The Telephone/DSL splitter DOES NOT split a single 1-line 2-wire connection.
Note:
On a standard telephone connection, a customer can have a maximum of two separate telephone lines/numbers. Line ONE is between (pins 2&3) of the RJ-11 connection. Line TWO (this only applies to customers who have requested a second line from the telephone company) would be between (pins 1&4).&
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.