Models of Pelco cameras that have been tested with version 3 NetBotz and BotzWare 4.X
Published date:
10 July 2020
Issue:
Models of Pelco cameras that have been tested with version 3 NetBotz and BotzWare 4.X
Product Line:
NetBotz
Pelco Cameras
Environment:
NetBotz NBWL0455 and NBRK0570
4.X botzware
Pelco camera support
Cause:
Not all Pelco cameras have been tested with NetBotz 4.0 botzware.
Resolution:
Please note that the NetBotz 3xx and NetBotz NBRK0450/0451 do not support the Pelco integration.
The initially supported Pelco cameras from version 3.x firmware are:
Pelco Camera Model
Product Family
Firmware Version Tested
IP3701H-2
IP
Unavailable
IP110-CHV9
IP110 Camclosure®
Unavailable
SD4N-W0
Spectra Mini IP
Unavailable
The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.0. The Sarix line of Pelco cameras have been added to testing:
Pelco Camera Model
Product Family
Firmware Version Tested
IXS0C
Sarix IX
1.7.19.9080-A1.5842
IXE20DN
Sarix Enhanced
1.7.19.9081-A1.5843
IX30DN
Sarix IX
1.7.8.9080-A1.5288
IMSOC10
Sarix IME
1.7.41.9260-O2.6725
SD4N-W0
Spectra Mini IP
1.2.15
With the release of Botzware 4.2, the following list of additional Pelco cameras and firmwares have also been tested:
Pelco Camera Model
Product Family
Firmware Version Tested
IMSOC10
Sarix
1.8.2
IM10C10
Sarix
1.8.2
IX30DN
Sarix IX
1.8.2
D5118
Spectra HD
1.8.2
TXB-N
Spectra IV IP
1.8.2
DD4N-W0
Spectra Mini IP
1.2.15
IP110
IP110 Camclosure®
1.0.47
IP3701
IP
1.0.10
The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.4:
Pelco Camera Model
Product Family
Firmware Version Tested
IM10C10
Sarix
1.9.2
IMS0C10
Sarix
1.9.2
D5118
Spectra HD
1.9.2
IME119
Sarix Enhanced
2.1.2.0.8280-A0.0
The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.5.3:
Pelco Camera Model
Product Family
Firmware Version Tested
IL 10
Sarix
Unavailable
The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.6.3:
Pelco Camera Model
Product Family
Firmware Version Tested
IJP121-1IS
Sarix
1.16.37
Important Note:
Pelco Sarix Pro models that were originally listed as supported do not correctly update the resolution settings presented to NetBotz appliances. NetBotz can no longer support Sarix Pro models due to this limitation of the Pelco camera and they have been removed from this compatibility matrix.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.