Browse FAQs

Removing supplemental OIDs from a version 3 Netbotz appliance may cause basic view to show invalid sensor.

Published date: 22 July 2020

Issue:

Removing supplemental OIDs from a version 3 Netbotz appliance may cause basic view to show invalid sensor.

Product Line:

NetBotz

Environment:

NetBotz version 3 appliances.

Cause:

Unexpected Configuration Change.

Resolution:

When a scanner on a version 3 Netbotz uses a supplemental OID and that OID is removed, you may see a sensor in it's place or under one of the other sensor sets in basic view that looks something like this: nbSNMPEnc2D5186C0_user_USER_3315_USER__0: --- This is a known issue and may be addressed in a future revision on Botzware. For the time being, the only way to remove this invalid sensor is to remove the scanned device itself and re add it. This does not effect the other sensors on the scanned device and is not see in the Advanced View software.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.