Browse FAQs



Why doesn't StruxureWare or ISX Manager's mass configuration feature update or show password credentials on APC Network Management Card devices?
Mass configurations of APC UPS ... done via ISX Manager or StruxureWare may ... ... Environmental Monitoring Unit 1 (AP9312TH) ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... : Metered/ Switched Rack PDUs ( ... Rack Automatic Transfer Switches (AP77XX, ... ... G Metered/ Switched Rack PDUs ( ... InfrastruXure Manager ... removed from the config .ini ... outside of the config .ini, ... This affects ISX Manager's ability to make mass configuration change of the various ... Because the ISX Manager takes one device's configuration file ... ... X, the config .ini
Netbotz / InfraStruXure Central supplemental OID configuration
... Netbotz / InfraStruXure Central supplemental OID configuration InfraStruxure Central InfraStruxure Central /Data Center ... When configuring Netbotz products to ... The OID below is a sample that would return the Battery Capacity of an APC UPS: ... The following shows the outlet state of an APC switched rack PDU (rPDUOutletStatusOutletState) for outlets 1 and 4: ... 1 .3.6.1.4.1.318.1.1.12.3.5.1.1.4.4
Configuring the Native Serial Shutdown Support in Windows 2000, XP, or 2003
How to Configuring the Native Serial ... Step # 1 : ... on Start > Settings > Control Panel ... ... on the system configuration . ... UPS tab to configure Windows to communicate ... ... NOT used to configure an APC USB ... The UPS service is currently stopped ... The UPS service , by default ... Once configured , the UPS service will start on ... ... button to begin configuration . Note 1 : ... that incorrect port settings may cause communications ... ... hardware/device manager . ... The proper port settings are: 1 Stop Bit ... save the new settings and start the UPS service , click Apply ...
How can I mass configure an Network Management Card (NMC) or NMC embedded product?
... can I mass configure or configure multiple Network Management ... ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... : Metered/ Switched Rack PDUs ( ... Rack Automatic Transfer Switches (AP77XX, ... ... G Metered/ Switched Rack PDUs ( ... AP44XX Automatic Transfer Switches . ... AP9312TH, Masterswitch 1 /2) ... ... card, mass configuration of those devices ... ... and uploading a single configuration file ( config .ini) ... ... Mode cannot be modified through the config .ini ... , these four settings will be disregarded ... ... keyword will not configure Output Voltage, ...
Why isn't Daylight Savings Time (DST) working properly when using custom settings and Network Time Protocol (NTP)?
... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... : Metered/ Switched Rack PDUs ( ... Rack Automatic Transfer Switches (AP77XX, ... ... Network Management Card 1 product family in ... ... daylight savings time setting and a NTP ... disregard the DST settings 90 seconds after ... ... ), Symmetra Single & Three Phase ... Network Management Card 1 devices (AP9617 ... Please download the new firmware from or through ISX Manager and StruxureWare Central update servers. If you are unable to upgrade, use the traditional daylight savings time setting .
Where can I get support for APC and MGE Products?
APC Enterprise Manager ... Assessment Services ... Battery Replacement Services ... Ethernet Switches ... InfraStruxure Manager ... Installation Services ... KVM Switches ... MGE Service Bypass ... MGE Static Transfer Switches ... NetBotz Central ... Network Integration Services ... On Site Service ... Operations Capacity Operations Change ... PowerChute Inventory Manager ... Project Management Services ... Rack-mount Transfer Switches ... Remote Monitoring Services ... Service Bypass Panel Service Plans ... Software Configuration ... Start-Up Service ... StruxureWare Central ... Switch Boxes Switched Rack PDU ... Training Services ... Wall-mount Transfer Switches
Changing the Line VRMS (Nominal Line Voltage) on your 208/230vac capable Rack Automatic Transfer Switch (ATS)
Go to 1 -Device Manager menu, 3-ATS Configuration and configure item 8-Line VRMS to 208 Important:
Video: Data Center Expert | How do I delete old data?
StruxureWare Central (SWC) StruxureWare Central (all versions ... Accessing Purge Settings ... Center Expert Purge Settings 1 ) Log into ... ... > Server Administration Settings > Storage Settings > Purge Settings Automatic Purge Settings ... percentage of total capacity that will initiate ... ... percentage of total capacity that will cause ... ... percentage of total capacity that will result ... Apply Purge Settings Click to save changes to the settings . ... Total Repository Usage identifies allotted capacity (size) and current usage (percentage) for each type of data stored in all repositories. ... tab, it only identifies capacity and usage for all remote repositories. ... menu > Server Administration Settings
Why can't I connect to my APC Network Management Card or embedded Network Management Card using a serial connection?
... Environmental Monitoring Unit 1 (AP9312TH) ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... : Metered/ Switched Rack PDUs ( ... Rack Automatic Transfer Switches (AP77XX, ... ... G Metered/ Switched Rack PDUs ( ... Rack Automatic Transfer Switches (AP44XX) ... ... at the correct settings ... for the default settings . ... rate CAN BE CHANGED ... user, a change to the configuration ... device like ISX Manager or StruxureWare Central . If you are having an issue connecting, try setting the baud rate to a different value: ... The unit will inform you of the baud rate change .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.