Browse FAQs



SurgeArrest - minimum install distance of 10 meters (30ft).
... and the electrical service panel . ... creation of a single UL standard for ... ... less, under one certification. ... ranging from Type 1 -5. Type 1 ... secondary of the service transformer and the ... side of the service equipment overcurrent device ... ... side of the service equipment overcurrent device ... at the branch panel and Molded Case ... ... from the electrical service panel to the point ... The distance (10 meters ... - Component Assemblies -,Component assembly consisting of one or more Type ... Type 1 , 2, 3 Component Assemblies ... Type 4 component assembly with internal or ...
Installation with Single / 2-Pole or 3/4 Pole MCB’s
... acceptable to use single pole for a single -phase installation ... it doesn’t make sense to modify the distribution board to accommodate other breakers types. First of all, it would require a major reworking of the way electrical panel boards are designed and manufactured , and since this has never been a problem, there’s no incentive to do this. To summarise, for countries where the earthing system is a TN-S or TN-CS, we can advise customers that a single or 3-pole breaker is permissible if it complies with
Are schematics available for APC products?
Service may require schematics ... ... APC does not distribute schematic drawings of ... ... undergone training for service of our products should attempt to service or repair an ... Distributing schematics of the ... ... chooses not to distribute schematic drawings and strongly advises against service of our products ... ... We do not distribute cable assembly schematics to the ... ... not attempt to manufacture your own UPS ... They can be reached on the web at https://coasttec.com/, or by phone at 1 -410-521-1000. ... For further information contact APC using any of the methods listed here:
acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
... hardware and ceiling panel required to extend ... ... hardware and ceiling panel required to extend ... Ceiling panel assemblies come with Lexan ... ... begin the ceiling panel ... recommend performing any service to 1 . Never work ... ... System; each panel is connected by ... completely remove each panel . ... the door frame assembly from the equipment ... ... strap (previously removed from the side ... 1 . Remove the ... 1 . Attach two ... Ceiling Panels ... Types of ceiling panels and required hardware The ceiling panels are configured in ... Ceiling panels are not intended ... ... not use ceiling panels to support power ... ... Preparing for ceiling panel installation
Rack PDU 2G (AP8XXX) Network Port Sharing Information
Rack Power Distribution ... ability to share one IP address via one network connection) ... PDUs using only one ... a number, 1 to 4, ... ... are connected to one another in a ... ... Rack PDU was manufactured prior ... Rack PDU was manufactured after ... " port of one of the grouped ... ... desired order, 1 to 4. ... ... have Display ID 1 . ... that have been removed from the group ... ... access to outlets 1 , 2, ... 3 on unit 1 , ... 2, outlets 1 through 6 ... , and outlets 1 ,2, ... APC- Service -Type = ...
AP8XXX Rack PDU 2G "NMC CAN Bus Off" Error
Rack Power Distribution ... For units manufactured later than December, 2012, you may find a CAN bus terminator pre-installed in one of these ports. ... If the source of the disruption is removed and no internal damage has occurred, the "NMC CAN Bus Off" error should clear on its own. ... Visually verify that everything is removed from the IN and OUT ports shown above.
Universal Transfer Switch (UTS) – FAQ
... to set Circuit 1 to UPS, ... Circuit 1 is tasked with ... Therefore Circuit 1 must be supplied ... ... opted not to manufacture the Auto- ... The UTS panel has the option ... ... APC UTS Automatic Remote Start/Stop ... * The panel comes preset to ... If the panel were to fail ... ... generator, the panel has a maximum ... A single 10 awg neutral wire would not be sufficiant to safetly complete the circuit. ... Two 10 awg neutral wires provide more than enough connectivity to meet the UTS panels needs, where as a single 8 awg wire is large and can be difficult to manipulate.
Connecting UPS Outputs Together (Paralleling UPS)
Paralleling output power of our units to one single phase distribution panel is not an option.
What are the basic troubleshooting steps for the Universal Transfer Switch model UTS6H?
The UTS was not installed at the recommended one foot distance from the building circuit breaker panel .
What are the basic troubleshooting steps for the Universal Transfer Switch model uts10bi?
The UTS was not installed at the recommended one foot distance from the building circuit breaker panel .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.