Browse FAQs



Can the horizontal cable troughs ar8008blk and ar8016ablk be used in conjunction with vertical cable managers ar7580a, AR7585 and AR7588?
Environment: All 750mm wide NetShelter SX cabinets: ar7580a, AR7585, AR7588, ar8008blk, ar8016ablk; all serial numbers.
Which NetShelter SX cabinet has a greater cable capacity, 750mm wide or 800mm wide?
For example; ar7580a is the high volume vertical cable manager used in ar3150 and ar3350, and also in ar3180g and ar3380g.
Can the vertical cable management fingers for 600mm wide NetShelter cabinets be installed into 750mm wide NetShelter cabinets?
Cause: The Compatibility Chart shows that these cable managers are not compatible with the wide SX or SV cabinets.
Can the horizontal cable side channel organizer be installed into a 600mm wide NetShelter SX, VX or SV cabinet?
... mounting rails of NetShelter SX 750mm wide cabinets. NetShelter Cable Management ... need to move cables horizontally from front ... in a 600mm wide NetShelter cabinet. ... the narrower 600mm wide NetShelter cabinets when paired with a cable manager like ar8603a. ... sections that allow cables to feed through ... ... two of the cable side channels. (4 cable side channels total ... ... of the cabinet cable side channels can ... ... notice that the cable manager will interfere with ... This issue can be overcome by installing the cable manager to the rear of the front rails so the cable fingers are facing inward.
Can vertical cable managers or 0U accessory rails be installed in the front and rear of a NetShelter SX cabinet?
Issue: Customers want to know if there is flexibility in installing vertical cable managers , or where to mount the 0U accessory rails.
Can ar7580a be installed into the 45U NetShelter SX?
Issue: We need to determine if the 42U finger-style vertical cable managers will fit into a 45U NetShelter SX cabinet.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.