Single Phase Symmetra XR Frame Compatibility
Single Phase Symmetra XR ... only with certain UPS systems. ... , not every single phase Symmetra XR ... compatible with every UPS system in the single phase Symmetra product ... ... Symmetra Power Array UPS : use any ... Symmetra RM UPS : SYRMXR4B4. Symmetra LX UPS : use any ... SYXR12 and SYXR4 cabinets are compatible only with the use of the DC cable adapter, SYOPT3, which is discontinued. ... : The maximum number of XR frames that can be supported by single phase Symmetra platform is 7. Symmetra LX systems with integrated XR cabinets can only communicate with 6 additional, external XR cabinets.