Browse FAQs



Cable Picture Degradation When Using an APC Coaxial Surge Protector
After connecting an APC device with Coax Protection , customer observes picture degradation or loss of digital channels. ... SurgeArrest , Protectnet, Back-UPS, Back-UPS Pro, APC AV line of products ... Standard dB available to a home is 14 dB. ... Therefore, if one has a VCR and TV with coax cable between ... Inserting a cable protector like an APC ... APC Coax protection has been tested from 30 MHz to 1 GHz. ... terminated cables from an electronics store ; such as Radio Shack. ... (available at many electronics stores ).
Where can I get support for APC and MGE Products?
For support on APC and MGE products please visit: http://www. apc .com/support/ ... APC CS APC Enterprise Manager APC ES APC RS ... Back-UPS Office ... Biometric Security ... Metered-by- Outlet Rack PDU ... Notebook Security ... Security Cameras ... SurgeArrest Essential SurgeArrest Home / Office SurgeArrest Notebook SurgeArrest Performance
Why is the Protection Working LED of an APC SurgeArrest, or SurgeProtector off?
illuminate: 1. The unit is powered off (for 7 outlet SurgeArrest strips only).
Proper installation of a telephone line into an APC product with telephone line protection.
... side of a telephone patch cable to the telephone jack in the ... jack on the APC product (" ... ""Wall outlet "" or ...
Rack PDU 2G (AP8XXX) Network Port Sharing Information
apc > phReading 3 ... ... rpdu2g interface ( Home ->Group ... ... Port Sharing and Outlet Groups/ Outlet Users ... To create an outlet group, you ... ... for both the APC Operating System ( ... Outlet Users Outlet users can be assigned outlets on any Rack ... group with switched outlets . The outlet users will be stored on the Host ... ... you can view outlets assigned to a ... Outlet users can be ... Device Manager > Outlet Manager web page ... ... PDU 4: Outlet #2 off ... See the Security Handbook for APC Network Management Cards ... ... with VSAs, outlets on guest Rack ...
Video: What does the Site Wiring Fault Indicator LED on my APC UPS or Surge Arrestor represent?
All 120v APC Back-UPS and SurgeArrest products ... -UPS and SurgeArrest products equipped with ... On APC UPS products this ... APC recommends that you ... If the outlet that the APC UPS unit is plugged into is not properly grounded or properly wired, the unit will attempt to absorb the excess voltage instead of redirecting it to ground. ... Therefore, in order to maintain your warranty and protection under APC's Equipment Protection Policy, be sure that the APC unit is only plugged into a properly grounded outlet where the Site Wiring Fault Indicator (SWF) light is not illuminated.
SurgeArrest - minimum install distance of 10 meters (30ft).
... between the electrical outlet and the electrical ... APC Surge Arrest products ... utilization equipment being protected . ... external short circuit protection . ... to the voltage protection rating ... UL96A "Lightning Protection Systems" specifications ... A Type 3 surge protection device is not intended for direct lightning protection , therefore it is tested beyond the potentially effected area. ... Ideally for residential use, Type 2 which is often referred to as "TVSS" protection should always be installed at the main electrical service entrance.
Recommendations for protecting a laser printer
What are APC's recommendations for protecting Laser Printers? SurgeArrest , Back- ... ... these devices, APC does not recommend protecting laser printers with ... The Laser Printer should not be plugged into a UPS's Battery Outlets OR in to its Surge Only Outlets . These low voltage situations may cause an APC Back-UPS to transfer to battery operation repeatedly, eventually exhausting the unit's internal battery unnecessarily. ... APC recommends a Smart-UPS series product that is sized for the maximum power draw of the laser printer as defined by the manufacturer.
How do I configure my RADIUS server to authenticate my APC Network Enabled device?
... set up with APC Network Management Card ... ... through testing, APC by Schneider Electric ... shortname = apc VENDOR APC 318 ... BEGIN-VENDOR APC ATTRIBUTE APC -Service-Type 1 integer APC VALUE APC -Service- ... VALUE APC -Service- ... VALUE APC -Service- ... # APC local radius authentication ... APC -Service- ... ... to access your APC product via RADIUS ... ... For example, APC part number ap7900 ... ... also allows specific outlets to have their ... ... login for specific outlets . VENDOR APC 318 ... BEGIN-VENDOR APC ATTRIBUTE APC -Service-Type 1 integer APC
Scripting with APC by Schneider Electric Switched Rack Power Distribution Units (PDUs)
... scripting or automating outlet control on Switched ... ... like to automate outlet control actions using ... APC by Schneider Electric ... scripting to automate outlet control. ... User Name : apc Password : apc ... you're typing for security purposes Outlets : 8 ... : ON : Outlet 1 ... : ON : Outlet 2 ... : ON : Outlet 3 ... : ON : Outlet 4 ... : ON : Outlet 5 6 : ON : Outlet 6 ... : ON : Outlet 7 ... : ON : Outlet 8 APC > ... , please contact APC by Schneider Electric ... ... Rack PDUs offer outlet control via Simple ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.