Browse FAQs



APC Schneider Cooling Unit Identification
APC Cooling Unit identification. All Cooling Units. All Product models , all serial ... Model ... W= Water Cooled ... F= Water Cooled ... D= Water Cooled ... G= Glycol Cooled ... B= Glycol Cooled ... P= Glycol Cooled Model ... coil C= Chilled Water Model C= Chilled Water ... In-Row Model ... Main C= Chilled Water Model ... W= Water Cooled ... G= Glycol Cooled BA=208 ... Model ... W= Water Cooled ... G= Glycol Cooled Model AFX 1 = 1 Bay ... Bay 06 ( 1 Bay) 08 ( 1 Bay)
What alarms can be automatically reset on a High Capacity Uniflair Unit
• Low Pressure • Circuit 1 Chilled Water High Temperature Threshold Exceeded
Will the EcoAisle replace the tradition HACS offering
For facilities leveraging air or water economizers this systems is adaptable to maximize free cooling hours.
What filter is being used for your InRow 300mm?
Data Center Cooling ... The filtration of conditioned air is extremely vital to maintaining the clean, particle- free environment required by electrical equipment. The system uses a <20% efficiency ASHRAE 52.1, 12.7 mm ( 1 /2 in) washable, deep loading, large dust-holding filter that meets HF- 1 standards for electronics (MERV 1 per ASHRAE 52.2). Model ... 1 acrc10x
Why choose glycol over water?
All cooling units that require heat exchangers ... All Product models , all serial numbers ... - Since glycol systems are closed and dirt- free , no sidestream or full flow filtration is required. ... - Did you know that just 1 /16" of scale reduces heat transfer by 40%!
What is the RDU’s entering water temperature guidelines
All Product models , all serial numbers ... 1 . What range of Entering Water Temperature should be supplied for the system? ... Typically if you chilled water source is starting to exceed its target set point, the chiller will alarm and begin to inform you of the problem as well.
UPDATED MARCH-2016: Unable to access my APC Network Management Card (NMC) enabled device via HTTPS (SSL/TLS)
... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... ... ACSCXXX, RACSCXXX Cooling Units (except ... acrc301h, acrc301s Cooling Units, ... who uses any one of the products ... One such example is ... ... future firmware update plans to address this ... ... Network Management Card 1 (NMC1) ... acrc ACRCXXXX InRow Chilled Water (except ... ... your local APC Cooling Support team) ... Automatic Transfer Switch models except ... your local APC Cooling Support team) ... ... your local APC Cooling Support team) ... ... your local APC Cooling Support team) ... ... a value of 1 to allow fallback ...
DAC, Cancoil Installation Manual
All Models Section 1 . Warranty and ... Section 1 . ... and dry and free of all debris ... ... are based on 1 degree per 100 ... ... a rate of 1 ” drop per ... ... a rate of 1 ” drop per ... ... and should have 1 additional trap per ... ... information regarding the model in question. ... the system with 1 /4” ... 1 . Check the supply voltage when the system is operating. ... The ambient fan cycling controls will maintain a condensing temperature of about 115 degrees whenever the outdoor temperatures are greater than the values shown above.
Why do I have an E4 error on the display NetworkAIR 1000?
Spot Cooling ... 1 ) Make sure the tank is empty, and the float at the top of the tank is free for movement ... If you press the switch in while the cooling mode is set up, the unit will turn on."
What are the basic troubleshooting steps for the Back-UPS Connect model bge50ml / bge50ml-CA?
For devices that can charge using input greater than 1 A make sure that the device is connected to the 2.4A USB ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.