Rack PDU 2G (AP8XXX) Network Port Sharing Information
... AP8XXX Rack PDU models ... ability to share one IP address via one network connection) ... PDUs using only one ... a number, 1 to 4, ... ... are connected to one another in a ... ... Sharing groups you plan to have. ... " port of one of the grouped ... ... desired order, 1 to 4. ... ... have Display ID 1 . ... 2: 40 W ... contact, basic model properties, firmware ... ... access to outlets 1 , 2, ... 3 on unit 1 , ... 2, outlets 1 through 6 ... , and outlets 1 ,2, ...