Browse FAQs



How can I resolve “Failed to create java virtual machine.” error when launching StruxureWare Data Center Expert client?
1 ) Navigate to ... Installation directory for StruxureWare Data Center Expert . (default ... C:\ Program Files (x86)\ StruxureWare Data Center Expert X.X ...
Why does StruxureWare Data Center Expert not accept my One Time passcode?
StruxureWare Data Center Expert is not accepting ... StruxureWare Data Center Expert StruxureWare Central / Data Center Expert all versions. SturuxureWare Data Center Expert requires a 64 ... passcode and the Data Center Expert's MAC address. 1 . In a ... AP9465 = StruxureWare Data Center Expert Basic ap9470 = StruxureWare Data Center Expert Standard AP9475 = StruxureWare Data Center Expert Enterprise AP94VMACT = StruxureWare Data Center Expert Virtual Machine SFDCOBASE = StruxureWare Data Center Operation ... a VM or Data Center Operation. ... all the relevant information . ... a word processing application such as notepad ... ... . Launch your Expert client.
Restoring StruxureWare Data Center Expert backup to a new Virtual Machine causes system to not fully boot up.
1 . Gracefully shut down the virtual appliance. 2. In your virtual server console, select the option to add a hard disk.
Before importing a backup from a StruxureWare Data Center Expert server to the Virtual Appliance version, configure the public and private network settings first in VMWare.
... backup from a StruxureWare DCE server to the Virtual Appliance version, ... StruxureWare Data Center Expert StruxureWare Data Center Expert Virtual Machine . ... configured with a single NIC can cause ... To avoid this issue, please set up the second NIC's configuration on your StruxureWare Central Virtual Appliance before restoring the backup. ... If you've already encountered this issue, you must go to the StruxureWare Central client and configure a different netmask. ... Log back into the StruxureWare Central client and then re set the correct network settings
Data Center Expert | How do hardware and software support contracts work?
... hardware warranty and software support contracts work for StruxureWare Data Center Expert . StruxureWare Data Center Expert (DCE) - Virtual Appliance (AP94VMACT ... StruxureWare Central (SWC ... StruxureWare Data Center Expert (all versions ... StruxureWare Central (all ... Software Support Contract StruxureWare Data Center Expert appliances come with 2 years of factory hardware ... software support . The Data Center Expert appliance and any ... active and complete software support in order to ... technical support and software upgrades. Software support contracts are required for ... covered under base software support SKUs) as ... ... not currently require support contracts .
Where can I find the manual for the StruxureWare Data Center Expert VM appliance?
Environment: StruxureWare Data Center Expert Virtual Machine
Trial version of StruxureWare Data Center Expert VM appears to have 25 nodes available.
Trial version of StruxureWare Data Center Expert appears to have 25 node license available. ... StruxureWare Data Center Expert ... The current default configuration of all StruxureWare Data Center Expert is that the system comes with a pre-installed 25 node license key. The Virtual Machine or VM version shows this same 25 node license key in the user interface however until activated, will only allow 5 nodes to be added to the system. ... It was done so APC did not need to add a 5 node key to just this one version.
StruxureWare DCE virtual machine may hang, logs show e1000 NIC error
Product Line: StruxureWare Data Center Expert
StruxureWare Central Virtual Machine time may drift by a few seconds a day.
Product Line: StruxureWare Central, StruxureWare Data Center Expert .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.