Browse FAQs



Where can I get support for APC and MGE Products?
Data Center Facility Cooling - Andover Continuum or TAC Vista ... High-Density Cooling Enclosures ... InfraStruxure for Large Data Centers InfraStruxure for Medium Data Centers InfraStruxure for Server Rooms InfraStruxure for Small Data Centers InfraStruxure for Wiring Closets InfraStruxure Manager InfraStruxure Type A InRoom Direct Expansion InRow Chilled Water ... On Site Service ... Portable Cooling ... Room Cooling Accessories ... Row Cooling Accessories ... Uniflair Chilled Water
On the RP Chilled Water the top piping connections have one pipe for the return plumbed to the top, but no supply pipe connection, is this normal?
Yes this is normal. In the crating of each unit will be two long extension pipes that is field installed and insulated.
What alarms can be automatically reset on a High Capacity Uniflair Unit
• Low Pressure • Circuit 1 Chilled Water High Temperature Threshold Exceeded
APC Security Advisory - InfraStruxure Central 5.0 Java Runtime Environment
... Security Advisory - InfraStruxure Central 5. ... InfraStruxure Central InfraStruxure Central version 5 ... InfraStruxure Central utilizes Java ... [ 1 ] ... some files and web pages ) or a ... ... downloaded from a website unauthorized access to ... some files and web pages ). InfraStruXure Central 5. ... InfraStruXure Central Server The InfraStruXure Central Client installer ... ... Also, although InfraStruXure Central does allow ... ... machines running the InfraStruXure Central Client ( ... ... , upgrade the InfraStruXure Central Server using ... The InfraStruXure Central Client uses one font throughout all ... The InfraStruXure Central Client installer ... Also, InfraStruXure Central does not ...
What are the operational conditions for an InRoom (Stulz) Unit
... conditions for an InRoom (Stulz) ... The InRoom precision air conditioning ... ... +/- 1 % Chilled water -/ cooling water pipes: Maximum water head pressure: ... ... piping between the cooling unit and the ... ... condenser and the cooling unit: 5 ... is below the cooling unit Entering water temperature (EWT) for CW coil: 7°C (44.6°F) Leaving water temperature (LWT) for CW coil: 12°C (53.6°F) ... Cooling fluid (DX): 30% Glycol ... Chilled water medium (CW): 0% Glycol
APC Schneider Cooling Unit Identification
APC Cooling Unit identification. All Cooling Units. ... FM Air/ Water /Glycol W= Water Cooled F= Water Cooled D= Water Cooled ... G= Glycol Cooled ... B= Glycol Cooled ... P= Glycol Cooled ... W= Hot Water ... coil C= Chilled Water C= Chilled Water ... Main C= Chilled Water W= Water Cooled ... G= Glycol Cooled BA=208 ... W= Water Cooled ... G= Glycol Cooled AFX 1 = 1 Bay ... Bay 06 ( 1 Bay) 08 ( 1 Bay) 28 (3 Bay ... W= Water Cooled
Video: How to set up load assist on a Uniflair unit.
Product line: Uniflair Gen 1 and Chilled Water Units.
Data Center Expert | How do hardware and software support contracts work?
... Details on how extended hardware warranty and software support ... InfraStruXure Central (ISXC ... InfraStruXure Central (all ... ... of factory hardware warranty and no ... can have hardware warranty up to a ... years of factory warranty . Factory warranty details and hardware extension SKUs are provided ... Year 1 Extended Hardware Warranty Statement of Work ... DCIM Assets website 1 ) Open the ... 1 ) A Base ... 1 Year Software Support SKU ... 1 Year Software Support SKU ... Software Support Example 1 ... 1 Year SKU ... 1 WMS1YRBASIC WMS3YRBASIC ... 1 Year SKU ... 1 WMS1YRSTD WMS3YRSTD 1 WMS1YR25N WMS3YR25N 2 wms1yr100n wms3yr100n ... 1 Year SKU ... 1 WMS1YRVM WMS3YRVM 2 WMS1YR25N WMS3YR25N 2 wms1yr100n wms3yr100n 1 wms1yr1000n wms3yr1000n
Stulz Tech Data Manual
ACPDX21-86, acpcw40-150, Tech Data Manual, Stulz, Chilled Water , Dx, Inroom
How do I install Pex piping?
Please see the attached documents for best practices and procedures for installation of Pex-Al-Pex chilled water piping. ... 1 . Do not allow plex to be exposed to sunlight for an extended period of time as this will have an effect on the integrity of the piping. ... 4. Each run from the CDU to the acrc1xx should be one continuous run, no joints and fittings.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.