Browse FAQs



Information for Colors of UPS Galaxy 5000, Galaxy 5500
Product line: Galaxy 5000 , Galaxy 5500
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
... Down the MGE Galaxy 5000 UPS Galaxy 5000 , Galaxy 5500 ... Powering Down the Galaxy 5000 UPS ... power down the UPS are available on ... ... is for a single UPS without an external ... Step 1 : Touch any button on the display to wake it up. ... Step 4: Choose “Stop the UPS ” ... At this point, the load is no longer protected by the UPS . ... The UPS is now fully isolated from the load. ... Step 6: Turn the Q 1 Switch to Off ... There is still stored energy in the capacitors, and batteries inside the UPS . Never remove any covers or panels.
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from total power ... Galaxy 5000 , Galaxy 5500 ... reasons, the Galaxy 5000 may be in ... ... commissioning a new UPS . ... of a new UPS must be performed ... ... to restore the Galaxy 5000 UPS from total power ... This procedure is for a single UPS without an external bypass panel. ... Step 1 : Set the input Q 1 switch to On Step 2: Wait until the end of the UPS initialization with PFC start-up. ... Step 4: Choose “Start the UPS ” ... The Inverter Assumes the load, and the UPS is normal operation with the load protected.
Information for Noise level of UPS Galaxy PW
UPS rating in KVA 100 130 150 180 200 225 Noise level on normal floor (dBA) 62 63 64 65 67 68
​Information for Noise level of UPS Galaxy 5000 NAM
UPS rating ( kVA ) 40/50/60/80kva 100/130kva Noise level on a normal floor (dBA) with ...
Galaxy 5000; Modbus Q1 Input Breaker status does not change state
The Q 1 Modbus register is only monitored on EMEA Galaxy 5000 / 5500 UPSs.
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
This assumes only one 66061 card or UPS or STS is connected to the enclosure but if more than one change as required.
Galaxy 5000, Galaxy 5500; Dust Covers
... has been determined that dust and other foreign conductive particles have been getting inside the UPS during shipping or from site construction projects during installation ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.