Technical FAQs

Ask a Question

How to reset the username or password in PowerChute Business Edition 9.5 and above
Issue User has forgotten their username or password created during the installation, and is unable to login to the PCBE Agent. Product PowerChute...
Video: Troubleshooting no communication between UPS and PowerChute Business Edition
Issue: No Communication with UPS Product Line: PowerChute Business Edition   Environment: All supported OS Cause: There are many possible causes....
Can I use a NetBotz NBPD0165 camera pod with older NetBotz appliances?
Issue: Can I use a NetBotz NBPD0165 camera pod with older NetBotz appliances? Product Line: NetBotz Environment: NetBotz cameras Cause: NetBotz has...
Why is my NetBotz 750 browser window hanging after upgrading the firmware from 5.0.1?
Issue: After upgrading NetBotz 750 firmware, the upgrade appears to hang. Product Line: NetBotz Environment: NetBotz 750 firmware upgrade. Cause:...
How do I serially connect to the NetBotz 750?
Issue: How do I serially connect to the NetBotz 750? Product Line: NetBotz Environment: NetBotz 750 serial port configuration and driver Cause: The...
NetBotz 4.6.3 e-mail "From" address shows as "Unknown"
Issue: NetBotz 4.6.3 e-mail "From" address shows as "Unknown" Product Line: NetBotz Environment: NetBotz version 4.6.3 firmware Cause: A change was...
Java Cryptography Extension requirement for SNMPv3 configuration in PowerChute Network Shutdown and PowerChute Business Edition
Issue: In certain geographies it is necessary to install the Java Cryptography Extension to use privacy protocols AES-192 or AES-256 in the PowerChute...
International Connectors & Country Comparison Reference Chart
Issue: International Connectors & Country Cross Reference Chart Product Line: N/A Environment: N/A Cause / Resolution:   Country Follows the Connectors...
What is the definition of the shutdown types in PowerChute Business Edition?
Issue: Need to know the different shutdown types in PowerChute Business Edition. Product Line: PowerChute Business Edition Environment: All supported...
Video: How to run PowerChute Network Shutdown setup wizard & configure for VMware ESXi hosts and vCenter Server
Issue: Need to setup PowerChute Network Shutdown for VMware ESXi hosts and vCenter Server. Product: PowerChute Network Shutdown v4.2 Environment:...
Results 1 - 10 of 100