Browse FAQs

Video: Connect Battery on Back-UPS RS/NS M2 & MS Series

Published date: 10 October 2019

Issue:
Tutorial for connecting or replacing the internal battery on Back-UPS Pro RS/NS M2 & MS series. The UPS will indicate a disconnected battery by flashing an empty battery icon on its front display.

Product Line:
Back-UPS Pro RS/NS

Environment: 
BR1000MS/BR1350MS/BR1500MS
BN1100M2/BN1350M2/BN1375M2/BN1500M2

Cause:
All APC UPS systems are shipped with batteries disconnected to comply with US DOT regulations. The UPS will flash the battery icon to indicate a disconnected battery state.
A severely discharged/damaged battery will also generate the flashing battery alert. The Back-UPS will not be able to recharge or otherwise use a severely discharged battery.

Resolution: 
To connect, disconnect or replace the internal battery, please follow the steps indicated in the video and images below.




Was this helpful?

What can we do to improve the information ?