Are the ACSC condenser fans always on? Are they variable speed?
Published date:
11 June 2020
Issue:
Are the condenser fans always on? Are they variable speed?
Product line:
ACSC100, ACSC101
Environment:
InRow Cooling Cause:
Resolution:
The condenser fans operate whenever the compressor is operating, otherwise they are off. They are continuously variable speed from 100% down to 30% in order to maintain a 425 psig refrigerant discharge pressure.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.