ISX-PDU; How to wire and configure the user input and output contacts via the User Connection plate
Published date:
07 May 2020
Issue:
How to wire and configure the user input and output contacts via the PDU User Connection plate
Product line:
ISX-PDU
Environment:
All models, all serial numbers
Cause:
User Connections to the PDU Monitoring Unit (Brains) is done thru the User Connection plate. User connections may be for EPO interface, input and output contacts.
Resolution:
Please refer to attached PDF files detailing the User Connection plate and how to configure the PDU user input and output contacts via the PDU PowerView display contacts screen.