Consulter la FAQ



Why doesn't StruxureWare or ISX Manager's mass configuration feature update or show password credentials on APC Network Management Card devices?
Mass configurations of APC UPS ... devices done via ISX Manager or StruxureWare ... ... , ap9340, NetBotz 200) ... Network Management Card 2 (NMC2) ... ... Network Management Card 2 include (but ... to): 2 G Metered/ ... ... removed from the config .ini ... outside of the config .ini, This affects ISX Manager's ability to make mass configuration change of the ... . Because the ISX Manager takes one ... ... X, the config .ini ... blurb from a config .ini: The config .ini file could be manually configured outside of ISX Manager to include ...
Video: How do I configure APC Network Management Card network settings?
... , ap9340, NetBotz 200) ... Network Management Card 2 (NMC2) ... ... Network Management Card 2 include (but ... to): 2 G Metered/ ... ... TCP/IP settings prior to being ... ... available options to configure the Network Management ... with it's initial settings : the Wizard ... ... based devices are configured for a boot ... ... it is not configured on your DHCP ... ... methods below to configure /access the ... ... Network Management Card 2 /3 ... Network Management Card 2 and 3 based ... higher, are configured for DHCP Only ...
How can I mass configure a Network Management Card (NMC) or NMC embedded product?
How can I mass configure a Network Management Card (NMC) or NMC embedded product? ... can I mass configure or configure multiple Network Management ... ... , ap9340, NetBotz 200) ... Network Management Card 2 (NMC2) ... ... Network Management Card 2 include (but ... to): 2 G Metered/ ... ... MasterSwitch 1/ 2 ) do not ... ... Card, mass configuration of those devices ... ... configuration file ( config .ini) ... ... Network Management Card 2 firmware v6 ... ... modified through the config .ini ... , these four settings will be disregarded ... ... keyword will not configure Output Voltage, ... ... I obtain a config .ini ... to retrieve the config .ini
Data Center Expert | Surveillance frame rate when NetBotz communication is SSL
StruxureWare Data Center Expert surveillance slows when communicating to NetBotz appliance(s) using SSL. ... NetBotz (series 300 and higher) ... NetBotz (all versions) ... Regardless of the frame rate you have set within the Data Center Expert surveillance settings , the maximum frame rate Data Center Expert will receive from a NetBotz appliance is 5 frames per second. ... This is working as designed . Without the encryption and decryption in SSL, surveillance frame rates will remain as configured . This issue effects both version 2 and version 3 NetBotz appliances.
NetBotz | Scheduling Periodic Reports
NetBotz v3 Wall ... NetBotz v3 Rack ... NetBotz v 2 and v3 As designed , Periodic Sensor ... ... this limitation and configure your appliance to ... ... the Advanced Scheduling settings and return to ... ... your Periodic Report settings . When you specify an interval of 1,440 minutes (1 day) the report will run once every day, at the time you saved the configuration .
Netbotz | What type of information can I see in a NetBotz SNMP trap?
... found in a NetBotz SNMP trap NetBotz NetBotz SNMP trap ... traps from a NetBotz device are a ... ... the same when configuring traps for StruxureWare ... the alarm action configuration for a trap ... ... a similar trap configuration but it is ... rather than the NetBotz OIDs. ... This article is designed to provide some ... VarBinding 2 : 1. ... ... .13 = 2 ... look at the NetBotz MIB, you ... that the trap parameters are listed under ... ... .netBotzAPC. NetBotz .netBotzTrapParms Please note that you NMS or trap receiver must support this type of nested trap in order to get this information from the NetBotz appliance.
Why can't I connect to my APC Network Management Card or embedded Network Management Card using a serial connection?
... , ap9340, Netbotz 200) ... Network Management Card 2 (NMC2) ... ... Network Management Card 2 include (but ... to): 2 G Metered/ ... Ensure you are connecting at the correct settings ... Please reference the product’s user manual for the default settings . ... by the user, a change to the configuration file, or a managing device like ISX Manager or StruxureWare Central. ... If you are having an issue connecting, try setting the baud rate to a different value:


Résultats 1 - 10 de 50

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.