FAQs Techniques

Poser une question

Filtre de Résultat

    Are the NetShelter SX Cabinets grounded per UL / IEC 60950, 61010-1 / 6.5.1.3?
    Issue: Customers require information on grounding NetShelter cabinets to IEC specifications.
    How do you install an Isolated Extension Cable with a Share-UPS?
    Issue Need assistance on installing the Isolated Extension Cable ( IEC ) with a Share UPS.
    Why would I need to use the 24VDC adapter when using the APC Isolated Extension Cable?
    ... signaling through an Isolated Extension Cable ( IEC ), you must use a 24VDC adapter to power the UPS End Unit of the IEC ...
    Why is there no serial cable included with my new Smart-UPS srt5kva -10kva
    Environment: SRT5KRMXLI, SRT5KRMXLIM, SRT5KRMXLT, SRT5KRMXLT- IEC , SRT5KRMXLW-HW, SRT5KXLI, SRT5KXLT, SRT5KXLT- IEC
    What is the Smart-UPS On-Line surge and spike test data?
    The Smart-UPS On-Line products have been tested to levels that exceed IEC standards for voltage spikes, voltage surges, and ...
    What is the IP (Internal Protection) rating of the NetShelter SX, SV and CX cabinets?
    The NetShelter cabinets have not been independently tested to IEC 60529 for Internal Protection, but they meet the rating scale (see below) ...
    Résultats 1 - 10 de 29