Consulter la FAQ



SurgeArrest - minimum install distance of 10 meters (30ft).
Do not install this device if there is not at least 10 meters (30 feet ) or more of wire between the electrical outlet ...
Cable length for APC Temperature Sensor - AP9512TBLK
Resolution The cable length is about 3.6 m (12 ft +/- 1 inch).
Why do I need refrigerant traps in my piping?
Data Center Cooling Q: Why are traps important every 20 feet of height?
APC Environmental Sensors FAQ
... wants to extend the length, APC engineers have extended the length using two 12 foot PS/2 extension cables with minimum measurement changes ...
What sensors are supported by the NetBotz Wireless Sensor Pod 180 (nbpd0180) ?
... Racks - 12 ft nbes0303 NetBotz Door ... Racks - 50 ft nbes0302 APC Temperature Sensor - 13 ft AP9335T APC Temperature ... Sensor - 13 ft (Only reports ...
How long are the intake and exhaust hoses on the acpa4000?
The exhaust hose is 10 FT X 8 IN and yes you may have them ducted through a wall.
What are the capabilities of the condensate pump on the ACSC unit?
... l/hr) at a maximum run of 50 ft (15.2 m) of which 16 ft (4.9 ...
What is the NetBotz smoke sensor nbes0307 sensitivity?
The nominal detection sensitivity for the nbes0307 is 2.5 percent-obscuration-per- foot .
Can I use Cat 6 cables to extend NetBotz sensors with RJ45 connectors?
... a cat5 coupler that enables the RJ45 connection to be extended to an extra 100 feet in most cases (see sensor specs for detail ...
Lighting calculation for Lighting Kit part numbers; acdc2018, acdc2019
We have to have a minimum of 50 foot candles at all racks/cabinets.


Résultats 1 - 10 de 66

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.