Технические часто задаваемые вопросы



What is the maximum number of rack access cards that can be configured in a version 3 NetBotz appliance for use with the rack access pod 170?
When using StruxureWare Data Center Expert to configure multiple NetBotz appliances, the limit in this system is also 200 cards and again all cards ...
NetBotz | Hardware & Software Support Information and Limits
... Year 2 Year 3 Year 4 Year ... ... years factory with 3 years of purchasable ... ... Appliance, except for consumables, such ... ... Year 2 Year 3 Year 4 Year ... NetBotz 200 The NetBotz 200 is limited to ... ... years factory with 3 years of purchasable ... ... year software support contract must be purchased ... ... Appliance, except for consumables, such ... ... Year 2 Year 3 Year 4 Year ... ... years factory with 3 years of purchasable ... ... year software support contract must be purchased ... ... Appliance, except for consumables, such ... Year 1 Year 2 Year 3 Year 4 Year 5 Year 6 Software Support Out of Support Hardware Support Factory Warranty Out of Support
Where can I get support for APC and MGE Products?
... 25 47251WH- 3 47251WH-5 ... 25 47251YL- 3 47251YL-5 ... 75 47279BL- 200 47279BL-75 47302gy-2M ...
Questions on where to ship 3 phase batteries for disposal
For disposal of batteries used in 3 phase product applications ... paid shipping labels for batteries that are ... year warranty or for batteries being replaced ... a specific battery contract .
Data Center Expert | How do hardware and software support contracts work?
... and software support contracts work for StruxureWare Data Center Expert. StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... Software Support Contract StruxureWare Data Center Expert appliances come ... The Data Center Expert appliance and ... Software support contracts are required for the server which ... ... currently require support contracts . Hardware Support Contracts StruxureWare Data Center Expert Appliances can ... ... must be continuous for the duration of ... Year 3 Software Support Contracts ... can be provided for trail installation of ... ... not be purchased for a virtual appliance ... ... local sales representative for purchase related questions ...
Video: Data Center Expert | Device Discovery for Third-Party Devices using SNMP
... Devices into Data Center Expert using snmpv1 ... StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... ... additional knowledge bases for discovering different other ... NetBotz 200 Series ... added into Data Center Expert to accurately ... Data Center Expert by default ... For more information, ... 3 ) Device Discovery ... ... the required information for device discovery. If the discovery will be for multiple devices that need to be within different groups, it is recommended to discover them into the Unassigned group. ... Check the Box for Run Discovery Now and click Finish. ... 3 ) Within the Device View pane, search for the IP Address of a device in question.
Video: Data Center Expert | Device Discovery for APC Devices using snmpv1
... Devices into Data Center Expert using snmpv1 ... StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... ... additional knowledge bases for discovering different other ... NetBotz 200 Series ... string (used for APC Device Priority ... ... - Application Version 3 .X- ... 3 ) Navigate to ... ... - Application Version 3 .X- ... ... 4) Data Center Expert requires the ... ... is an entry for Read and another for Write and that ... ... Type will work for both Read ( ... ... Host Name fields for the applicable entries ... to DCE. For a description of ... ... perform mass configurations for the device( ...
Data Center Expert | Device Discovery for APC Devices using snmpv3
... Devices into Data Center Expert using snmpv3 ... StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... ... additional knowledge bases for discovering different other ... NetBotz 200 Series ... - Application Version 3 .X- ... 3 ) Navigate to ... ... - Application Version 3 .X- ... ... settings that Data Center Expert can use for communication. ... - Application Version 3 .X- ... ... Host Name fields for the applicable entries ... For a description of ... ... perform mass configurations for the device( ... For example, limit ... have all wildcards for the IP Range ... ... discovery will be for multiple devices that ...
NetBotz 200 shows phantom sensors when multiple dry contact cables are connected.
NetBotz 200 shows phantom sensors when multiple dry contact cables are connected. ... NetBotz Rack Monitor 200 ... Issues have been seen where adding 3 or more dry contacts to a NetBotz 200 appliance directly or per pod can cause one of the sensors to replicate. It has been seen where 4 dry contacts may be listed while only 3 are connected. Other strange occurrences have been seen such as phantom alerts for contact closure when none exist. This appears on NetBotz Firmware v3.5.6 (Rack Monitor 200 ) as well as earlier versions ... firmware for the NetBotz 200 .
NetworkAIR FM 3-Way Valve Flow Pattern
This document describes the NetworkAIR FM 3 -Way Valve Flow Pattern. ... Proper set up for three way valve operation ... Below are the Port designations and configurations to provide a clear understanding of the 3 -Way valve position during operation . ... 200 psi Maximum Close Off ... Floating is standard on the on/off actuators and allows use with three wire output controllers. ... This input signal allows the actuator to accurately position the valve ball from full open to full close for maximum flow.


Результаты 1 - 10 of 63

Не нашли то, что искали?

Обратитесь к нашей команде по обслуживанию клиентов для получения информации о технической поддержке, помощи в составлении претензий и другого.