Технические часто задаваемые вопросы



Data Center Expert | How do hardware and software support contracts work?
... for StruxureWare Data Center Expert . StruxureWare Data Center Expert (DCE) StruxureWare Data Center Expert (all versions ... StruxureWare Data Center Expert appliances come with ... The Data Center Expert appliance and any ... ... required for the server which has a default 25 nodes (covered under ... as each additional node license . Modbus license keys and surveillance keys do not currently ... StruxureWare Data Center Expert Appliances can have ... Model Appliance ... virtual machine activation key (AP94VMACT) ... ... can put your server and license keys back under support ... ... amount of Device Nodes Installed ... number of install licenses .
Data Center Expert | What virtualization environments are supported?
You can purchase a license key to upgrade to ... monitor additional device nodes and activate supported ... migrate from a server hardware version to a virtual ...
Data Center Expert | Why does StruxureWare not accept my One Time passcode?
StruxureWare Data Center Expert is not accepting ... StruxureWare Data Center Expert (DCE) ... StruxureWare Data Center Expert (all versions ... SturuxureWare Data Center Expert requires a 64 character license key that is created ... and the Data Center Expert's MAC address. StruxureWare Data Center Expert (DCE) ... ... this, the server registers itself in ... ... notifies the DCE server that there is ... ... Afterwards, the server scans the unit ... ... when purchasing a license key is not the actual license . ... passcode to a license key . ... add a new server , please click ...
Data Center Expert | Migrating from a Physical Appliance to a Virtual Appliance
... a DCE hardware server to a virtual server ? StruxureWare Data Center Expert (DCE) StruxureWare Data Center Expert (all versions ... ... As the data center is moving away from hardware servers and towards vitalization ... ... a virtual DCE server , there are ... ... the AP94VMACT activation key to activate the ... ... as the hardware server from which you ... ... if your previous server already has licensing on it ( ... base 25 device nodes and 1 surveillance node ) your will ... ... do not have access to your company's ... ... than the hardware server . License keys are tied to ... on the new server .
Video: How do I register a passcode for NetBotz or StruxureWare?
StruxureWare Data Center Operation (DCO ... StruxureWare Data Center Expert (DCE) StruxureWare Data Center Operation (DCO ... StruxureWare Data Center Expert (DCE) When purchasing licenses for these products ... and not a license key . ... to get a license key . ... After purchasing a license key for NetBotz or ... ... that already has license keys installed, your ... ... user that has access to the account ... ... what type of license key you are redeeming ... either: Data Center Expert Model , NetBotz Model , or SFDCOBase (Data Center Operation). ... select the options key and then redeem ...
Data Center Expert | Trial version VM appears to have 25 nodes available.
... Machine or VM version shows this same 25 node license key in the user interface however until activated, will only allow 5 nodes to ...
Can I transfer license keys between StruxureWare Data Center Expert servers?
Product Line: StruxureWare Data Center Expert (DCE)
Data Center Expert | Getting Started
... with a Data Center Expert Appliance. StruxureWare Data Center Expert (DCE) StruxureWare Data Center Expert (all versions ... ... the Physical Data Center Expert Appliance ... the Virtual Data Center Expert Appliance ... restricted to 5 nodes . ... you have purchased licensing , continue to ... the passcodes for licenses . ... the StruxureWare Data Center Expert Virtual Appliance? ... storage that Data Center Expert has within VMWare ... Getting Data Center Expert on the Network ... that your Data Center Expert (DCE) ... ... for StruxureWare Data Center Expert StruxureWare Data Center Expert Security Information ( ... Licensing and Software Support
Video: Data Center Expert | How do I enable surveillance for NetBotz cameras?
You can verify the licensing that you have installed by going to: System Menu > Server Administration Settings > License Keys .
Data Center Expert | Working with SSL Certificates (Self-Signed, CSR, & CA Authority)
Being updated will prevent a private key mismatch that will prevent the server from being able to be access via HTTP/HTTPS.


Результаты 1 - 10 of 69

Не нашли то, что искали?

Обратитесь к нашей команде по обслуживанию клиентов для получения информации о технической поддержке, помощи в составлении претензий и другого.