Технические часто задаваемые вопросы



APC Schneider Cooling Unit Identification
FM Air / Water /Glycol FMXXX- XXX - XXX Capacity KW Air Pattern ... Expansion A= Air Cooled E= Air Cooled W= Water Cooled F= Water Cooled D= Water Cooled ... W= Hot Water ... -CXX- XXX Capacity KW Air Pattern ... C= Chilled Water ... -CXX- XXX ... -CXX- XXX Capacity KW Air Pattern ... C= Chilled Water Capacity KW Air Pattern ... C= Chilled Water ... -XX- XXX Capacity KW Air Pattern ... Main A= Air Cooled W= Water Cooled ... -XX- XXX -X
How to navigate through an Network Air FM unit display
... through an Network Air FM unit display ... ... ACFM, Network Air , ir40. ... FM DX Precision Air Conditioner. ... ® (chilled water ) and DX ... ... of the return air and the dew ... ... of the return air . ... humidity of the room air . ... point in the room . If the room temperature is 23 ... ... point of the room is 26° ... ... between the actual room dew point and the desired room dew ... to control the room environment or if ... Air Filter. ... the type of air filters installed in ... either standard ( 30 -40% ... Air
Network Air FM unit spare parts list
... 4183 Glycol/ Water LL ... 4182 Glycol/ Water & Air LL ... ASSY FM 35 KW DX ... ASSY FM 40 KW DX ... ASSY FM 50 KW DX A16- 30 -10- ... a40- 30 -10- ... a30- 30 -10- ... ... A9- 30 -10- ... Filter Air 30 % UF & ... Filter Air 85% UF ... ... FM35-50 KW W/ AIR DEFLECTORS ... FM35-50 KW W/ AIR DEFLECTORS ... FM35-50 KW W/ AIR DEFLECTORS ... FM35-50 KW W/ AIR DEFLECTORS
What are the operational conditions for an InRoom (Stulz) Unit
... The InRoom precision air conditioning units operate ... Room Conditions: Chilled water -/cooling water pipes: Maximum water head pressure: ... ... unit and the air cooled condenser: ... Return air conditions for evaporator ... Return air conditions for cooling ... Entering water temperature (EWT ... Leaving water temperature (LWT ... ... DX): 30 % Glycol ... G): 30 °C ( ... Chilled water medium (CW): 0% Glycol ... Downflow units with an external static pressure: 20 Pa (0.08 in w g) Upflow units with an external static pressure: 50 Pa (0.20 in w g)
EcoBreeze Variable Speed Drive Technical Spec’s
Assembly style With heat sink Motor power kW 15 kW ... flux vector control with PWM type motor ... ... ... 30 V ≤ 100 ... ... torque 100 % with braking resistor continuously ... ≤ 150 % with braking resistor for ... ... , input voltage 30 V max , ... input voltage 30 V max , ... ... 5 A at 30 V DC, ... ... 2 A at 30 V DC, ... ... .100 mA with PLC , impedance ... ... % without dripping water conforming to IEC ... Ambient air for storage - ...
DAC, Cancoil Installation Manual
Air Cooled Condenser DAC Air Cooled Condensers For ... Cancoil air -cooled condensers ... As with all refrigeration equipment ... ... file a claim with the shipping company ... ... place a claim with the shipping company ... ... under the chassis with a forklift or with a spreader bar ... ... be used if air -cooled quipment ... ... contractor in accordance with applicable codes and ... ... purge the system with dry nitrogen during ... ... be pitched downward with a rate of ... On systems with parallel compressors or systems with cylinder unloading, ... ... should be sized with a 20% ... ... be pitched downward with a rate of ...
Why choose glycol over water?
There is a one-time initial cost to fill the system with 30 -40% glycol.
What is the maximum kW rating for the NetShelter SV?
The SV was not designed to have a removable roof or any roof fans or chimney, but as long as the cooling in the room is sufficient there is no reason why a customer could not load the cabinet with 5kw of equipment. However, without adequate air exchange there may be some hot spots.
Network Air FM Field Fix Solution Chemical Propeties and MSDS Sheet
Residual product will be rinsed away with condensate water and leave a hydrophilic fin surface.To
Water leak in DataCenter.
Just simply clean it out occasionally. Run a wire, flush with water , or blow air through it to clear the clog.


Результаты 1 - 10 of 83

Не нашли то, что искали?

Обратитесь к нашей команде по обслуживанию клиентов для получения информации о технической поддержке, помощи в составлении претензий и другого.