Технические часто задаваемые вопросы



Netbotz | What type of information can I see in a NetBotz SNMP trap?
VarBinding 5 : 1.3. 6 .1. 4 .1.5528 ... 100.11. 6 = nbAlinkEnc_0
HTTP/HTTPS Web Access does not work in v6.X.X firmware but works on v5.X.X in certain NMC2 configurations/environments
... certain users have found that web interface ... ... upgrading from v 5 .X. ... Users using a fresh install of v 6 .X. ... ... accessing NMC2 over a WAN connection or VPN or other types of "remote ... APC has discovered a v 6 .X. ... ... been investigated and a fix is being ... ... resolved with AOS 6 . 4 .0 ... work, as a test. ... downgrade to v 5 .X. ... show a change, then standard troubleshooting steps should be verified such as verifying general networking connectivity, proxy settings, IP address, ...
Data Center Expert | Discovering a ModbusTCP device
Process to discover a Modbus TCP device ... ... knowledge bases for discovering different other types of devices: 3 ) Select Modbus ... 4 ) Enter the ... 5 ) Select a compatible Device Type from the list ... ... need to obtain a Device Definition File ... 6 ) Select the ... ... 8) Choose a device group to discover the device into ... ... group that you discovered the device into ... ... still trying to discover the Type will be " ... ... Failed Modbus TCP Discovery ... 11) Newly discovered Modbus TCP devices will show a status of Normal when first discovered .
Data Center Expert | Discovering a NetBotz 300-500 Series Appliance
Process to discover a NetBotz 300, ... NetBotz v 3 Wall Appliance: ... (nbwl0355/ 6 ) & 455 ... (nbwl0455/ 6 ) NetBotz v 3 Rack Appliance: ... ... knowledge bases for discovering different other types of devices: Discovering a NetBotz 300- ... 3 ) Select the Device Discovery Type of NetBotz Appliance ... 4 ) Enter the ... ... to longer device discovery times. 5 ) Enter the ... 6 ) Select the ... ... to the Device Discovery screen and then ... ... Device Group to discover the NetBotz Appliance ...
NetBotz v3 | How do I configure a PCNS Shutdown alert action?
... Process for creating a PCNS Shutdown alert action on a v 3 NetBotz Appliance. NetBotz v 3 (355, ... NetBotz v 3 (firmware 4 . 5 . 4 and higher) ... until NetBotz v 4 . 5 . 4 . ... download can be found in knowledge base ... 3 ) Select the ... 4 ) Click Add 5 ) Select Send ... 6 ) Enter a name for this ... ... active 24 hours a day, 7 days a week. a ) Click Advanced ... To disable a time range, ... To enable a time range, ...
Data Center Expert | Discovering a NetBotz 700 Series Appliance
Process to discover a NetBotz 700 series ... ... 750 (firmware 5 .2. ... ... knowledge bases for discovering different other types of devices: ... required to add a NetBotz 700 series ... ... Requirements for SNMP Discovery ... settings can be found in knowledge base ... If a root password has ... be used in a later step for ... 3 ) Log into ... ... choose to create a new user ( ... 4 ) Log on ... Discover NetBotz 700 Series ... 3 ) Click on ... 4 ) Click on ... ... the 700 series discovery . 5 ) Click Next ... you wish to discovery into.
Which DHCP options are used when an APC Network Management Device makes a dhcpv4 request?
... Management Device makes a dhcpv4 request? ... , you will find a list of dhcpv4 ... /receive in a DHCP Request/ ... ... following options within a valid DHCP response ... ... optionally identify the type and configuration of a DHCP client. ... - This option type is most useful ... When a reserved client contacts ... identifier value to a corresponding identifier used ... ... is used by a DHCP client to optionally identify the type or category of ... it represents. A - AOS 5 .1. 5 and above ... following options within a valid DHCP response ... ... - (option 3 )
Video: What are the different sensitivity settings of a Smart-UPS?
... sensitivity settings of a Smart-UPS ... ... Smart-UPS detects line voltage distortions ... ... looks at these three parameters (THD ... ) and makes a quantitative analysis based on all three things using a proprietary algorithm. ... operate online during a wider array of ... ... length of time a Line-Interactive ... ... If you experience a load drop during ... ... UPS such as a Smart-UPS ... ... event of any type of voltage disturbance ... ... generally 2- 4 milliseconds. ... the event of a RMS voltage- ... ... the continuity of a computer's operation. ... They are generally 6 -8 milliseconds ...
Can I plug my APC Rack-Mount Power Distribution Unit (Rack PDU) into a feed receptacle located in the under floor plenum? (Also applicable to Configurable & Modular Power Distribution)
... Article 645. 5 clearly states that ... ... and certain cable types are allowed under ... 645. 5 Supply Circuits and Interconnecting Cables ... be connected to a branch circuit by ... ... not to exceed 4 . 5 m (15 ... ... be permitted under a raised floor, ... ... nonmetallic conduit, Type MI cable, Type ... cable, or Type AC cable. ( 3 ) Supply cords ... with 645. 5 (B) ... ( 6 ) "Cables ... ... be listed as Type DP. Type DP cable having ...
NetBotz | Reformatting a Version 2 or 3 Appliance
Reformatting a Version 2 or 3 Netbotz Appliance NetBotz v 3 Wall Appliance: ... (nbwl0355/ 6 ) & 455 ... (nbwl0455/ 6 ) NetBotz v 3 Rack Appliance: ... ... password) on a NetBotz V2/V 3 300, 400 ... ... 1: Open a web browser 3 : You will ... 4 : After it ... you will see a message on the ... ... If you have a V2 appliance, use a null modem serial ... ... If you have a V 3 appliance, use a USBA-USBB ... ... 2: Start a serial communications application ...


Результаты 1 - 10 of 74

Не нашли то, что искали?

Обратитесь к нашей команде по обслуживанию клиентов для получения информации о технической поддержке, помощи в составлении претензий и другого.