Технические часто задаваемые вопросы



StruxureWare Central reports NetBotz sensor values when the device is actually offline
Issue: StruxureWare Central reports NetBotz sensor values when the device is actually offline
PowerChute Business Edition 9.x agent does not launch properly from StruxureWare Central
Issue: PowerChute Business Edition 9.x agent does not launch properly from StruxureWare Central
Unexpected Average/Peak Calculations if StruxureWare Central and Monitored NetBotz Clocks Not Synced.
Issue: Unexpected Average/Peak Calculations if StruxureWare Central and Monitored NetBotz Clocks Not Synced.
StruxureWare Central iPhone app launches to private side devices using the same protocol used to log in to the server.
Issue: StruxureWare Central iPhone app launches to private side devices using the same protocol used to log in to the server
Why does ISX Manager/StruxureWare Central display the incorrect Kilowatt value when utilizing the Physical Layout or ISX Operations feature for my Metered/Switched Rack PDU product?
APC has identified a problem that causes the Physical Layout or StruxureWare Central Operations to display the incorrect Kilowatt (kW) value.
How to change a RAID battery on the StruxureWare Data Center Expert Enterprise server?
Product Line: StruxureWare Data Center Expert StruxureWare Central
Can StruxureWare Data Center Expert output a 32 bit register with its Modbus output?
Product Line: StruxureWare Central / StruxureWare Data center Expert
StruxureWare Data Center Expert will not mount to a share using NTLM version 2
Environment: StruxureWare Central / Data Center Expert any version 7.2.7 and earlier


Результаты 1 - 10 of 50

Не нашли то, что искали?

Обратитесь к нашей команде по обслуживанию клиентов для получения информации о технической поддержке, помощи в составлении претензий и другого.