Технические часто задаваемые вопросы



Data Center Expert | Surveillance frame rate when NetBotz communication is SSL
... have set within the Data Center Expert surveillance settings, the maximum frame rate Data Center Expert will receive from a NetBotz appliance is 5 ...
"This device is running an unsupported firmware version" when discovering NetBotz 750 With StruxureWare DCE 7.7
The release dates for DCE 7.7 and Botzware 5 .2 have been staggered so ... this message which relates only to surveillance .
Video: How do I retrieve surveillance clips in StruxureWare Data Center Expert
Retrieving surveillance clips in StruxureWare ... NetBotz NetBotz discovered by DCE and licensed for surveillance ... assistance in retrieving NetBotz camera clips in ... ... go to the Surveillance perspective. ... thumbnails for your NetBotz Appliances that are ... If a thumbnail shows a red circle with a cross-line through it, the camera has not been licensed for surveillance . ... Clips are stored according to the NetBotz Appliance date/time, not the DCE Appliance date/time. 5 ) Within the Choose Date section, select either Relative or Date Range.
NetBotz 750 / 755 Captured clips shows duration and frame rate as per previous video capture settings
Captured clips shows duration and frame rate as per previous video capture settings on NetBotz 750 / 755 ... NetBotz 700 series ... This issue may be seen in StruxureWare Data Center Expert's surveillance data for the 700 series appliance with the issue. ... 5 . Resolve the alarm (Do not delete the alarm configuration)
Do alerts in StruxureWare DCE that come from the NetBotz 750 include images?
... come from the NetBotz 750 include images ... NetBotz 750 NetBotz 750 5. ... ... 2 and 3 NetBotz such as the NetBotz nbwl0500, nbrk0570 ... The NetBotz 750 (considered version 5 NetBotz ) is discovered ... to how the NetBotz 250 or an ... ... this article, NetBotz 750 and it's ... ... releases that support surveillance are released ( ... alerts such as door opened etc are planned to trigger surveillance capture. So although there will be no images in the alerts themselves, there should be images available in surveillance .
Data Center Expert | Discovering a NetBotz 700 Series Appliance
... to discover a NetBotz 700 series appliance ... NetBotz 750 (nbrk0750 ... NetBotz 750 (firmware ... NetBotz 200 Series NetBotz 300-500 ... ... to add a NetBotz 700 series appliance ... SNMP Monitoring and Surveillance (cameras) ... ... ) Ensure the NetBotz appliance is accessible ... ... session to the NetBotz 750 using SSH ... ... on to the NetBotz Web User Interface ... Discover NetBotz 700 Series Appliances ... ) Click on NetBotz Appliance Credentials and ... 5 ) Click Next ... are not using Surveillance Cameras on the ... Add the NetBotz 700 Series SSL ... ... to add the NetBotz Appliance SSL certificate ... ... the Device > NetBotz Appliance Communication Settings


Результаты 1 - 10 of 52

Не нашли то, что искали?

Обратитесь к нашей команде по обслуживанию клиентов для получения информации о технической поддержке, помощи в составлении претензий и другого.