Browse FAQs



What is the expected life of my APC UPS battery?
F) rise in temperature will cut the battery life in half. A battery which would last for 4 years at 25 °
Why is my equipment dropped or rebooted while connected to my Smart-UPS?
F) rise in temperature will cut the battery life in half. A battery which would last for 4 years at 25
What are the factors that affect Battery Rated Service Life?
... factors that affect Battery Rated Service Life ... ... On paper, batteries are given a ... ... Smart UPS, Battery ... manufacturer says the battery is capable of ... ... things that affect battery service life. ... The standard is 25 C (77 ... ... temperature of the battery , and not ... ... in mind if batteries are installed inside ... temperature of the battery is usually 2 ... CAUTION: Battery life is halved ... °C above 25 °C. ... how often the battery charges and discharges ... 4 )Environment ... - The VRLA battery is specifically designed ... ... manufacturer says the battery is capable of ...
Matrix UPS will not perform a runtime calibration
1. Battery capacity must be 100% at start of calibration (all packs must indicated as float). 2. Initial "Estimated Run Time" must not exceed 128 minutes (remove battery packs if necessary). 3. Load must be above 25 %. 4 . Load must not fluctuate more than ± 5%. ... 5. The UPS must be allowed to run down to 25 % battery capacity.
Why is my actual UPS runtime different from the quoted runtime on the APC web page?
... Age of the battery ... - A new battery will only reach ... Temperature & battery life ... capacity of a battery will increase at ... Celsius rise above 25 deg Celsius. Recharging the battery ... - Whilst a battery will recharge to ... ... because as the battery approaches its fully ... back into the battery . ... capacity of the battery , reducing with ... ... - When a battery is stored, ... ... exceeded the typical battery manufactures specification the battery will return to ... Typical maximum storage period is 12 months at 25 deg Celsius, 8 months at 30 deg Celsius and 4 months at 40 deg Celsius.
Configuration and troubleshooting of E-Mail in PowerChute Business Edition Server
2. Type the IP address of the SMTP mail server and type in the # 25 in the Port Name field, then press connect. ... 3. Type Open <IpAddress> 25 (where <IpAddress> represents the IP address of your SMTP server). ... 4 . In order to test the email functionality, a manual test is required. A manual test will consist of putting the UPS on battery by removing input power.
acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
... , or XR Battery Cabinet is receiving ... 3. Know the procedure for disconnecting electricity to the PDU, UPS, or XR Battery Cabinet, in case of an emergency. 4 . Wear appropriate personal protective equipment. ... 6. Always follow local and site regulations when working on the PDU, UPS, or XR Battery Cabinet. ... Do not remove the rear doors of the UPS, PDU, or XR Battery Cabinet ... 3. Attach the plinth blocks to the enclosures, using four M8 × 25 -mm screws
Can I mix old and new batteries in a Smart-UPS?
... When replacing the battery cartridges in this ... , the two battery modules for the ... together and the four battery modules for the external battery pack should be ...
What is the maximum number of XR frames allowed with a Symmetra PX 20, 40 and 80kw solution?
There are 4 Battery Units in a Module this equals an XR frame with 32 Battery Units installed.
Matrix-UPS run time theory
Three of the four battery constants are set depending on the battery type (i.e. lead acid).


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.