Vented opening for airflow, temperature, and humidity sensors.
2
Network link LED
Shows the status of the network connection. Blinks to indicate network traffic (green = connected at 10 Mbps; yellow = connected at 100 Mbps).
3
Power LED
Indicates whether the unit is receiving power (green = receiving power; dark = not receiving power)
4
Camera LED
Blinks steadily when the integrated camera is active.
5
Alert LED
Indicates the alert status of the system. When more than one alert exists, the most severe will be indicated.
- Flashing once every eight seconds = Informational
- Flashing one very four seconds = Warning
- Flashing once every two seconds = Error
- Flashing once every second = Critical
- Flashing twice per second = Failure
6
Temperature display
- Displays the current temperature from 0 to 99 in Centigrade or Fahrenheit. The Temperature reading comes from the internal temperature sensor. If the temperature exceeds 99, the display will flash 99.
- When the unit first receives power, displays the unique identifier number for one minute.
- If an alert exists, flashes at the same rate as the Alert LED.
- During firmware upgrade, displays 88.
7
Lens housing
Must be removed to change the focus of the integrated camera.
Physical Description - Back
Item
Description
1
Sensor ports (4)
Used for connecting APC by Schneider Electric sensors, third-party dry-contact sensors, and standard third-party 0-5 V sensors. Third-party dry-contact state sensors require the NetBotz Dry Contact Cable (NBES0304). Standard third-party 0-5 V sensors require the NetBotz 0-5 V Sensor Cable (NBES0305).
2
10/100 Base-T network port
Provides for a 10/100 Base-T network connection and power through Power-over-Ethernet (PoE). (The appliance operates at 100 Base-T only.) Status and link LEDs indicate network traffic:
- Status LED: blinks orange and green at start-up, then indicates the status of the network connection (solid green = IP address established; blinking green = attempting to obtain an IP address).
- Link LED: blinks to indicate network traffic (green = connected at 10 Mbps; orange = connected at 100 Mbps).
3
USB port
Used to configure the appliance.
4
Reset
Used to restart the appliance.
The complete NetBotz 455 Installation and Quick Configuration Manual can be found here.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.