Browse FAQs

How can I reset the NetBotz 750 to defaults?

Published date: 18 October 2019

 

Issue:

How to reset the NetBotz NBRK0750 or NBWL0755

Product Line:

NetBotz

Environment:

NetBotz Version 5 appliances

Cause:

If the NetBotz appliance becomes inaccessible via the web and can not be accessed or if there appears to be corruption which you feel could be resolved by a full reset of the appliance, follow the below procedure.

Resolution:

If you can access the NetBotz appliance via SSH, connect using a utility such as putty.exe and when prompted, log in using root and the password you had provided upon initial root login (done via serial connection), then when prompted to press enter within 5 seconds, type a capital X. At the linux prompt type:

/netbotz_app/reset.sh
As of version 5.2.1, this command will change to:
/netbotz_app/factory_reset.sh

If you can not access through SSH, connect using the micro USB serial configuration cable. Once connected, verify you're using the correct port in device manager, then use the following settings and connect with a terminal emulation program such as Hyper-terminal or Putty:
115,200 Baud rate
8 Data Bits
No Parity
1 Stop Bit
No Flow control.

Open the connection and hit enter until prompted for a login.
Log in using root and the password you had provided upon initial root login (done via serial connection), then when prompted to press enter within 5 seconds, type a capital X and hit Enter.

At the linux prompt type:

/netbotz_app/reset.sh
As of version 5.2.1, this command will change to:
/netbotz_app/factory_reset.sh

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.