Browse FAQs

Video: How to change the Temperature and Humidity Alarm thresholds on a Uniflair unit.

Published date: 22 July 2020

Issue:
How to change the Temperature and Humidity Alarm thresholds on a Uniflair unit.
 
Product line:
All Gen 1 Uniflairs with push button displays and all Chilled Water Uniflairs.
 
Environment:
Push Button Display Uniflair units and all Chilled water Uniflair.
 
Cause:
Install, Repair Maintenance.
 
Resolution:

 

Press the PRG button.
 
Press ENTER on the Settings Menu.
 
Press ENTER on passcode if required 00000.
 
Press ENTER on Operative settings.
 
Use the Arrows to scroll to Alarm Settings.
 
Press the ENTER button to get to the desired setting that needs to be changed.
 
Use the Arrows to change the settings.
 
Press ENTER to go back to the top of the screen.
 
Press ESC back to the main screen.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.