Browse FAQs

PowerChute Network Shutdown v3.1 & 4.0 Required VMware vSphere Permissions

Published date: 04 August 2020

ISSUE:
What vSphere permissions are required by PowerChute Network Shutdown v3.1, and 4.0 for VMware?
Product Line:
PowerChute Network Shutdown v3.1 & 4.0 for VMware
Environment:
vCenter Server 5.x
ESXi 5.x
Cause:
Permissions required by PowerChute Network Shutdown when performing VMware related functions.

Resolution:

The attached PDF outlines the permissions required by PowerChute Network Shutdown to carry out the tasks below:
Deploying PowerChute Virtual Appliance
Creating the vCenter Plug-in
Creating and triggering vCenter Alarms
Virtual Machine Migration
Virtual Machine Shutdown/Startup
vApp Shutdown/Start
Putting Hosts in to maintenance mode
Shutting down Hosts
This allows you to create a service account role for PowerChute in vSphere instead of assigning the Administrator role which has full privileges.

NOTE:
The 3 system permissions listed on page 6 of the PDF are not configurable via vSphere Client GUI when connected to vCenter Server via Permissions tab . They are assigned automatically to any new user role that is created.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.